2024-04-24 07:47 PM
Having trouble connecting to ST-Link Utility. Cannot connect to target keep popping up.
Here is the schematic.
I`m using ST-Link/V2 for programming.
I followed this pinout to connect to the MCU
I connected the following. SWDIO to TP3, SWCLK toTP2, NRST to TP4 then VCC and Ground. I already double check connection and tried different board and I still can`t connect.
2024-04-24 08:41 PM
Hello @jeecrnl and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you to try using the STM32CubeProgrammer since the ST-LINK UTILITY is not recommanded for new designs.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-24 11:57 PM
Its having the same problem