cancel
Showing results for 
Search instead for 
Did you mean: 

STM32C0116-DK - On-board ST-Link failed after update process

Loic_C137
Visitor

Hello,

 

I have a brand new STM32C0116-DK evaluation board (official) and I fear I just bricked the on-board ST-Link :\

 

I wanted to run an example (blink LED) from the CubeIDE provided examples. When I pressed run, a popup displayed to notify me the ST-Link firmware should be updated. So I launched the process but the popup window freezed. I closed CubeIDE and disconnected the USB cable... Now the ST-Link LED is blinking RED at about 0,5 Hz and Windows doesn't detect any USB device at all (nothing is enumerated in device manager, nor a "USB device not working properly" popup) I think I did a mistake...

I will need it to work from home home for the two weeks. Is there a way I can force it to pass in update mode? I only have this board at hand right now, so is the only ST-Link debugger I have (had)...

1 REPLY 1
KnarfB
Principal III

Its not so easy to brick the board...

STM32CubeProgrammer is IMHO the most reliable tool for accessing a board including ST-LINK updates.

 ST-Link LED is blinking RED at about 0,5 Hz

This happens when power is on, but no USB comm. Try to reset the USB port / repower the computer.

hth

KnarfB