cancel
Showing results for 
Search instead for 
Did you mean: 

STM32C0116-DK has I2C pinout discrepancy

Karl Yamashita
Lead III

 

I am currently ordering the STM32C0116-DK to start developing some FW before getting the shipment. I've also sent the pinout to the EE team so they can start the schematic and laying out the PCB 

 

I started the project using the Board Selector. I've set up the UART and I2C which the pinout is shown below. The I2C peripheral is using PA9 and PA10

KarlYamashita_0-1727748659848.png

 

However, when I set up a new project using the MCU selector, the I2C peripheral are on other pins. I am selecting the same MCU where it shows the STM32C0116-DK as the development board to use.

KarlYamashita_2-1727749211922.png

 

But when I set up the I2C peripheral, it uses PB7 and PC14

KarlYamashita_5-1727749461949.png

I thought I could maybe remap the pins but there is no option for I2C on PA12 pin as shown below.

KarlYamashita_6-1727749648972.png

 

 

So which pinout is correct? Or are they actually 2 different MCU's? 

 

 

 

 

 

 

 

 

 

 

 

 

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

Same chip. In the SYS tab, remap the pins to PA9/PA10. After that, you can select the I2C1 functions for the pins.

TDK_0-1727751108061.png

 

TDK_1-1727751224191.png

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Guru

Same chip. In the SYS tab, remap the pins to PA9/PA10. After that, you can select the I2C1 functions for the pins.

TDK_0-1727751108061.png

 

TDK_1-1727751224191.png

 

If you feel a post has answered your question, please click "Accept as Solution".

Ahh! That's the first time seeing swapping pins using check box. Or maybe I've just never noticed.

Thanks TDK!

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.