cancel
Showing results for 
Search instead for 
Did you mean: 

stm32 nucleo-64 boards screw hole location

Licx
Associate III

How to get the height difference of these two screw hole?

Licx_0-1704181456446.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

There are several ways to determine the desired difference. One would be to read it from the GERBER data as recommended by @Tesla DeLorean. Another is to determine the difference from your screenshot, because all the values required for the calculation are given (typically, technical drawings do not specify each individual dimension, but use chain dimensions):

  • left hole:
    • CN8.6: Y = 0
    • CN8.1: Y = 0 + 5*2.54 = 12.7
    • CN6.8: Y = 12.7 + 5.08 = 17.78
    • CN6.1: Y = 17.78 + 7*2.54 = 35.56
    • left hole: Y = 35.56 + 13.97 = 49.53mm
  • right hole:
    • CN9.1: Y = 0
    • CN9.8: Y = 0 + 7*2.54 = 17.78
    • CN5.1: Y = 17.78 + 4.06 = 21.84
    • CN5.10: Y = 21.84 + 9*2.54 = 44.7mm

Difference = 49.53mm - 44.7mm = 4.83mm

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2

Perhaps check Gerber Drill file under CAD Resources tab for product 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Peter BENSCH
ST Employee

There are several ways to determine the desired difference. One would be to read it from the GERBER data as recommended by @Tesla DeLorean. Another is to determine the difference from your screenshot, because all the values required for the calculation are given (typically, technical drawings do not specify each individual dimension, but use chain dimensions):

  • left hole:
    • CN8.6: Y = 0
    • CN8.1: Y = 0 + 5*2.54 = 12.7
    • CN6.8: Y = 12.7 + 5.08 = 17.78
    • CN6.1: Y = 17.78 + 7*2.54 = 35.56
    • left hole: Y = 35.56 + 13.97 = 49.53mm
  • right hole:
    • CN9.1: Y = 0
    • CN9.8: Y = 0 + 7*2.54 = 17.78
    • CN5.1: Y = 17.78 + 4.06 = 21.84
    • CN5.10: Y = 21.84 + 9*2.54 = 44.7mm

Difference = 49.53mm - 44.7mm = 4.83mm

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.