2024-07-28 10:05 AM
It looped at a location deprived of access, waited a second, and returned to the same action. I thought STM32 was about programming.
Solved! Go to Solution.
2024-08-01 07:55 AM
Point taken. My problem was the invasive fashion of the installation. I appreciate that STM32CubeProgrammer cleaned the area and even changed some things without asking or alerting - it felt a positive impact. But I cannot consider this an installation: it took 48 hours, as long as I could bear a CPU-hog and whirling circle-icon sticking to the mouse cursor. Then I terminated STM32CubeProgrammer. I couldn't work.
2024-07-28 10:12 AM
Which cpu ?
Which st-link ?
+
Show pic, what CubePrg. telling:
like this
2024-07-28 11:04 AM
I think this is a complaint about the forum software, not the STM32 hardware, but it's hard to tell with such limited info.
Some links are broken, yes, but complaining without describing what you're looking for isn't going to get you anywhere. We're not mind readers.
2024-08-01 07:55 AM
Point taken. My problem was the invasive fashion of the installation. I appreciate that STM32CubeProgrammer cleaned the area and even changed some things without asking or alerting - it felt a positive impact. But I cannot consider this an installation: it took 48 hours, as long as I could bear a CPU-hog and whirling circle-icon sticking to the mouse cursor. Then I terminated STM32CubeProgrammer. I couldn't work.