2023-11-03 02:49 AM
I'm using my V3PWR probe for weeks now... but this morning it refuses to work. It was working yesterday evening with the same setup.
When I connect to the USB-C cable, no led at all , no USB enumeration ... nothing !! I changed the cable without success.
Where could I find the hardware schematics to have a chance to track the fault ?
Is there a point of failure already identified on these probes ?
Solved! Go to Solution.
2023-11-07 03:15 AM
Hello Christophe,
2023-11-03 08:28 AM
Hello @PJEN ,
If you don't get anything when you connect the probe to the pc it is most probably bricked if the LEDs are not lighting up and you tried replacing the cable and USB port i recommend you can return it to your vendor and look for a replacement.
Where could I find the hardware schematics to have a chance to track the fault ?
answer : you cannot find the schematics because they are not publicly diffused .
Is there a point of failure already identified on these probes ?
answer : there is not reported issues with this kind of problem on the STLINK-V3PWR so probably an electric spike was transferred to the device from the pc due to a sudden loss of power lead to the breaking of the probe.
BR
2023-11-07 02:26 AM
Hello @PJEN ,
Could you please let me know if you already returned back your STLINK-V3PWR to your vendor?
If not, I will contact you in private message to manage the replacement in order to analyze the failure directly in our labs.
BR,
Christophe
2023-11-07 03:15 AM
Hello Christophe,
2023-11-17 09:22 AM
Hi Pierre,
Your failing STLINK-V3PWR board has been analyzed in our labs:
So you do not have made anything wrong with your STLINK-V3PWR.
BR,
Christophe
2023-11-20 01:37 AM
:thumbs_up:
And I just received the replacement probe ...
Thank you for your support