2021-10-19 07:26 AM
Hi
Setup:
Destination µC running and connected with STLINK-V3MINI. When I plug the USB cable, the destination µC gets reset.
With ST-LINK/V2 this doesn't occur.
Schematics for the STLINK-V3MINI aren’t available so it's hard to debug.
Any suggestions welcome. Thanks!
2021-10-19 08:41 AM
I see the same behavior. NRST goes low for ~250ms 1.4ms. Surely it's being driven low by the firmware.
Power it first, then plug in the connector.
2021-10-19 08:51 AM
I use the ST-Link as debug interface – in combination with tools like STMStudio or some Python scripts (pyelfwrapper). The ST-Link is integrated in the housing and fix connected to destination µC.
If a problems occurs I want to plug in the USB cable and do some analysis with STMStudio. But with the reset all information is lost.
@ST Engineers:
If this is really done by firmware, please change this behavior. Thanks
2021-10-25 02:27 AM
We will use a "hardware" solution here using pin 22 (5V power from USB). The reset signal is only valid if pin 22 is high.