2018-12-12 05:40 AM
Hello there,
I have just obtained the STLINK-V3 device:
I have installed the STM32Cube Programmer (v 1.3.0) *** the drivers that comes along with it. The problem is that I cannot find the device:
There is no drivers missing, the device manager is "clean". I am using windows 10 64 bit version. Also there is no COM port available in the device manager.
According to the TN1235, this is correct:
I would appreciate all help.
2023-09-27 07:59 PM
Having the same issue 5 years on perhaps something where you lead with specific detail of your situation.
Like what drivers are actually loaded against the ST-LINK/V3, and what ST-LINK/V3 are we talking about.
Solution: Get the right drivers loaded, make sure Windows recognizes the device, that you have the right cable, not a charger / power-only one.