cancel
Showing results for 
Search instead for 
Did you mean: 

STLINK-V3 not recognized

Hello there,

I have just obtained the STLINK-V3 device:

0690X000006CoGyQAK.jpg

I have installed the STM32Cube Programmer (v 1.3.0) *** the drivers that comes along with it. The problem is that I cannot find the device:

0690X000006CoH8QAK.png

There is no drivers missing, the device manager is "clean". I am using windows 10 64 bit version. Also there is no COM port available in the device manager.

According to the TN1235, this is correct:

0690X000006CoIkQAK.png

I would appreciate all help.

10 REPLIES 10

Having the same issue 5 years on perhaps something where you lead with specific detail of your situation.

Like what drivers are actually loaded against the ST-LINK/V3, and what ST-LINK/V3 are we talking about.

Solution: Get the right drivers loaded, make sure Windows recognizes the device, that you have the right cable, not a charger / power-only one.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..