cancel
Showing results for 
Search instead for 
Did you mean: 

STlink V3 connections.

CSopk.1
Associate II

I want to be sure of the interconnects between the STlink and STM32 that will give me full debug capability using the CUBEIDE development environment. It would require 4 connections; 3.3v,gnd, SCLK(PA13) and SDIO(PA14). Some STM docs identify two additional signals NRST and TRACESWO. As I understand it the two additional signals are not necessary for full debug. Please confirm thanks.

11 REPLIES 11