2017-10-15 12:42 PM
I have a Nucleo STM32F446RE board, which I purchased less than a month ago.
After flashing it several times, I am now getting errors in flasher. I also checked my board with the STLink Utility.
When I press 'Verify blank' I am getting a message 'Can not read flash memory beyond address 0x08056000. Flash memory located below this address is blank.'
Also, occasionally, when I press 'Erase chip', the STLink Utility hangs and I have to restart it and the board.
I suppose this might be because the flash memory is worn out? But how can that be, if I have been using my Nucleo board for less than a month?
I have not done any flash programming from within my code, and I barely made more than 50 program cycles on my board.
I tried updating the STLink firmware (using STLink Utility), tried connecting to the board holding the 'Reset' button pressed, tried restarting the board multiple times (by disconnecting/connecting power)
Normally I am using this flasher utility:
https://github.com/texane/stlink
Has anyone had similar problems?
Thanks for your responses!
#stm32 #stlink2017-10-15 1:40 PM
Do you have other things plugged into, or connected to the board?
2017-10-15 2:14 PM
The problem was a bad charger, which introduced a lot of noise when I was flashing my nucleo. It somehow damaged the memory, and after several unsuccessful attempts STLink Utility managed to erase memory, since then everything seems to be working.