Skip to main content
Louie88
Senior
February 12, 2025
Solved

ST-Link V3 not detected in Mac M2

Hi,

I had to install STM32 tools on a MacBook Pro 2023 M2. I have a STM32H7474I-Disco board which works fine under Windows 11. When I connect the evaluation board to MacBook it pops-up a window to enable ST-Link driver. I enabled the driver but the usual new STL-Link USB drive with demo links does not appear in Finder... 

STM32CubeIDE (Programmer) reports no ST-Link is connected to MacBook. I am using the same USB cable as in Windows with an USB Type-A to Type-C adapter which works with all the external USB sticks, HDs.

I installed, STM32IDE, MX and Programmer and they seem to work right but the ST-Link V3 is not found.

When I connect the STM32H7474I-Disco board to MacBook Pro M2 then the LCD of the discovery board blinks 3-4 times (not enough power?) then stay on and runs my demo app just fine. Interesting...

Do you have any idea wha I did wrong?

Thanks,

Louis

 

This topic has been closed for replies.
Louie88
Louie88Best answer
Senior
February 13, 2025

Hi STTwo-32,

I borrowed an STM32H723ZG Nucleo board and I connected it with the same USB C to A converter and the same USB cable to the MacBook and I found the same: ST-Link still was not recognized...

Because we did not have other USB-C Hub we used our 8 (++) years old "no name" (i-Tech or something like that) USB 3.0 Type-A Hub (with 10-100 LAN port). The original Samsung USB C to A adapter (came probably with Samsung Galaxy S10 phone) was STILL connected one the USB C port of the MackBook Pro. The USB 3.0 Type-A Hub was connected to the adapter and the STM32H7 discovery/nucleo board was connected to the HUB.

And voila, with this complicated connection the MacBook recognized the ST-Link and STM32CubeIDE/Programmer recognized the ST_Link device. Everything worked just fine.

Who understands this? (I attached a picture about the complicated test setup).

So, my advice to everybody who runs into the same problem with Mac OS computers is: try to use a minimum USB 3.0 (or higher) USB HUB to connect STM development boards to USB C port of MacBook or MacOS computers.

Thanks for all help.

Louis

Ui.: Sorry, I forgot the picture...

9 replies

STTwo-32
ST Technical Moderator
February 12, 2025

Hello @Louie88 

I suggest you to take a look at this FAQ. It should be helpful.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Louie88
Louie88Author
Senior
February 12, 2025

Thanks, but it happens on MacBook Pro M2 (with latest MAC OS) not Windows. The Type-A to Type-C adapter is tested with many USB sticks/drives on that Mac including an 512GB Samsung M2 external SSD. I do not think this is a Type A to C adapter issue.

Louis

 

STTwo-32
ST Technical Moderator
February 12, 2025

The article is not tooking about a adapter issue or a problem on only windows PCs. Please read the article carefully and try all proposed work arounds. I think they should be helpful.

Best Regards. 
STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Louie88
Louie88Author
Senior
February 12, 2025

The mitigation suggestions in the referred post:

  1. Try to connect to another USB Type-C® port on your computer if available. Alternatively, using a USB Type-A port of your computer usually solves the issue. Done. MackBook Pro has 3 identical high speed USBC ports. None of them works with ST-Link V3.
  2. Connect the STLINK-V3 via an external USB High-Speed hub to the USB Type-C® port of your host computer (tested hub reference: Anker332 5in1). I can't do this but the USB-A to C adapter works with every high speed memory sticks, hard drives, SSDs we have. All the peripherals work fine with this MacBook Pro using the same USB Type A to C adapter.
  3. Use a different standalone probe to connect to your target board: ST-LINK/V2, STLINK-V3PWR, Segger J-Link. No chance, we do not have external ST-link adapters, like many others in this forum.

I do not know what else I could try. It is hard to believe that STM32H7474I-Disco board was not tested with a MacBook.

Louis

 

Louie88
Louie88Author
Senior
February 12, 2025

Hi STTwo-32,

Just two short facts:

  1. The same USB cable, the same Type A to C adapter and the same Discovery board (I used with MacBook) just work fine without any problem in 3 years old (not brand new) Windows 11 Notebook PC in a USB Type C port. This proves that the issue is not in the cable, nor in adapter and nor with USB speed.
  2. The ST-Link V3E port is a pure high-speed USB 2.0 port. Any not older than 8 years USB type A to C adapter must work. (ST32H7474I-Disco manual on page 14.

Thanks,

Louis

Louie88
Louie88AuthorBest answer
Senior
February 13, 2025

Hi STTwo-32,

I borrowed an STM32H723ZG Nucleo board and I connected it with the same USB C to A converter and the same USB cable to the MacBook and I found the same: ST-Link still was not recognized...

Because we did not have other USB-C Hub we used our 8 (++) years old "no name" (i-Tech or something like that) USB 3.0 Type-A Hub (with 10-100 LAN port). The original Samsung USB C to A adapter (came probably with Samsung Galaxy S10 phone) was STILL connected one the USB C port of the MackBook Pro. The USB 3.0 Type-A Hub was connected to the adapter and the STM32H7 discovery/nucleo board was connected to the HUB.

And voila, with this complicated connection the MacBook recognized the ST-Link and STM32CubeIDE/Programmer recognized the ST_Link device. Everything worked just fine.

Who understands this? (I attached a picture about the complicated test setup).

So, my advice to everybody who runs into the same problem with Mac OS computers is: try to use a minimum USB 3.0 (or higher) USB HUB to connect STM development boards to USB C port of MacBook or MacOS computers.

Thanks for all help.

Louis

Ui.: Sorry, I forgot the picture...

Associate
June 11, 2025

I also had to "downgrade" my USBC to USBA adapter to an old USB hub LogiLinkUA0139, and now I can connect to STLINKV3 from my mac M2. Thanks for the tips!

Andrew Neil
Super User
June 11, 2025

@jsola  So that does sound like the issue described in this article:

Possible communication failure between STLINK-V3 and some recent computers

 

@Louie88 that was the FAQ linked by @STTwo-32 to start with.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
June 11, 2025

@Andrew Neil Indeed. I tried with two different hubs now, and it works with both.