cancel
Showing results for 
Search instead for 
Did you mean: 

st-link/v2 - Programming Error

liberamos
Associate II
Posted on March 02, 2015 at 14:17

Hello,

i'm trying to load an .hex file into an ARM

STM32F103R6 with St-link/V2

 but there is something that doesn't work (see attached img).

Could you help me pls?

#st-link/v2-programming-issue
4 REPLIES 4
Posted on March 02, 2015 at 17:25

Says the erase failed. Guess I'd look at the board for issues, either design or construction. No real detail provided.

Does a bulk/mass erase work independently of the download?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
liberamos
Associate II
Posted on March 02, 2015 at 17:37

Thanks a lot for reply.

The board is good, we tried programming some PCBA with Keil uViusion4 and Keil uLink2 and all works good.

I tried to erase the chip with STM32 ST-Link Utility and it work fine, then i tried to erase sectors and some sectors is not erased (the system tell me ''Verify the memory protection'').

Posted on March 02, 2015 at 17:54

If the ST-LINK has current firmware, and it's not a SWD/JTAG issue, or one of the other connection options, you'll need to find someone at ST to discuss the issue with you.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
liberamos
Associate II
Posted on March 03, 2015 at 11:03

OK, I'll contact ST.

thanks a lot.