cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK V2 Clone cannot upgrade firmware, so cannot proceed with STM32CubeIDE 1.9.0

wb0gaz
Senior

Here is a sequence of screen captures demonstrating the problem I'm encountering (in particular, the firmware version displayed by the software appears to become same as the firmware version intended for upgrade; the upgrade says it failed, but then appears to complete, but does not actually solve the operational issue (subsequent attempt to use the device yields the following message in the console:)

"Error in initializing ST-LINK device.

Reason: ST-LINK firmware upgrade required. Please upgrade the ST-LINK firmware using the upgrade tool."

0693W00000LxQEzQAN.png0693W00000LxQEuQAN.png0693W00000LxQEaQAN.png0693W00000LxQEVQA3.png

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

now STM32 supports the clone stlinkV2 for debugging.

thanks