2016-09-21 7:21 PM
I recently completed a Seminar about the Cortex-M7 and when I got home, I updated my ST-Link Utility from 3.8.x to 4.0.0.0. The earlier version worked, the new version crashes every time I try Target -> Connect.
I also, did an ST-Link Firmware update and it still crashes. Any ideas? #st-link-crash-v4.0.0 #st-link-windows-10-crashSolved! Go to Solution.
2016-12-08 7:57 AM
This is a closing followup to this problem.
Last month, a virus changed the firmware inside my disk drive, changing the geometry from 500GB to 1.2MB and left behind a bootable version of FreeDOS. So my system was obliterated.
I handed the disk over to a security firm for investigation and it is now with a government security agency.
I bought a new disk and did a complete re-install of everything and the reported problem with ST-Link no longer exists.
In addition, STMicroelectronics has listened and made a dramatically impressive improvement to the community forum service that can only get better as time goes on.
Most excellent change folks and shows that your corporation is committed to the customer and continued use of your products.
2016-09-21 8:23 PM
2016-09-22 1:46 AM
Hi,
Could you please provide more details on your case: Have you an Error message ?If you can test and check this issue with another Pc, in order to know the root cause and deduce if the problem here seems related to the hardware or software environment or was caused by ST-Link.May be you can check if you are already setting compatibility mode for windows 8 option.Regards
2016-09-22 10:18 AM
Below and attached is a description of the failure modes with ST-Link Utility v4.0.0.
I apologize for the forum formatting, it did not properly translate the MS Word Tabs on the bullet lists. There are pictures in the attached file.Successful Operations
STM32 ST-Link Utility
All three different techniques for Connecting and Disconnecting were used,
Repeatedly Connect and Disconnect the following Targets,
All three different techniques for Connecting and Disconnecting were used,
Unsuccessful Operations
STM32 ST-Link Utility
The following two different techniques for Connecting and Disconnecting were used,
Repeatedly Connect and Disconnect the following Targets,
This is where it gets interesting,
TWICE
�?.ONCE
�?OK button in the Settings dialog window is used a Target Connect occurs without a CRASH
and all three Connection techniques continue to work as expected for the entire duration the ST-Link Utility application is run. When the application is exited, then the previously described failure mode occurs again as described.2016-09-23 3:41 AM
Hi,
Maybe this is due to synchronization problem in the web:
When I downloaded the version 4.0.0 without login (by simply providing name and e-mail address) I have the version 3.9.0 (sized 18Mb) instead the latest one.
But, when I downloaded with login, I have successfully installed
ST-Link Utility v
4.0.0So, you should
login before to downloadthe needed version ST-Link Utility and check that you have the version 4.0.0 (not 3.9.0) with size 24Mb.
Please try the download with login and let me know if it is OK with this suggestion.
Regards2016-09-23 6:15 AM
I always login before writing and when downloading.
The details in my entry also indicate the specific versions of the ST-Link software I am using and what the fault observation is. Thanks for the suggestion. ON ANOTHER NOTE, THE FORUM SOFTWARE NEEDS SOME REALLY MAJPR IMPROVEMENTS. I WOULD CONTEND THAT ST MICROELECTRONICS PRODUCT SALES ARE BEING ADVERSELY IMPACTED BY CRAPPY FORUM SOFTWARE. THERE ARE MANY OTHER VENDORS OFFERING ARM BASED MCU'S AND THEY HAVE SUPERIOR FORUM SOFTWARE APPLICATIONS.GET WITH THE PROGRAM ST MICROELECTRONICS. FIX THE FORUM SOFTWARE, NOW
.2016-12-08 7:57 AM
This is a closing followup to this problem.
Last month, a virus changed the firmware inside my disk drive, changing the geometry from 500GB to 1.2MB and left behind a bootable version of FreeDOS. So my system was obliterated.
I handed the disk over to a security firm for investigation and it is now with a government security agency.
I bought a new disk and did a complete re-install of everything and the reported problem with ST-Link no longer exists.
In addition, STMicroelectronics has listened and made a dramatically impressive improvement to the community forum service that can only get better as time goes on.
Most excellent change folks and shows that your corporation is committed to the customer and continued use of your products.