cancel
Showing results for 
Search instead for 
Did you mean: 

ST-link utility v. 4.0 and STM32CubeMX v.4.20 Bug

antonioB
Associate II
Posted on April 04, 2017 at 09:54

hi to all, i update the firmware of my  the my stm nucleo L152RE with st-link to the version

'ST-link firmware update V2.J27.M15 STM32 Debug+Mass storage'  and

later i update STM32CubeMX to 4.20 version

i use the cube mx to configure the gpio, when i configure RCC and RTC i see that the system crashes

i see the compiler crashes when arrived in this point

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

  {

    Error_Handler();

  }

the system go in Error_Handler();

I use old example, i created it one month ago, i don't open CubeMX i use only IAR for open the project but

now this example don't work and i see the compiler crashes when arrived in this point:

 if (HAL_RTC_Init(&hrtc) != HAL_OK)

  {

    Error_Handler();

  }

the system go in Error_Handler();

if i use old firmware, ST-link firmware update V2.J20.M4 STM32 Debug+Mass storage my old example work well.

excuse me for my bad english

best regards

Antonio

#bug #stm32cube #st-lik-utility #stm32l152re
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Imen.D
ST Employee
Posted on April 04, 2017 at 10:27

Hi

Buonanno.Antonio

,

This is confirmed bug in RCC clock configuration with

CubeMx 4.20 and will be fixed soon

in the new patch release.

The issue occurred due to this error line:

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;

and y

ou should replace it

with the following line that will resolve your problem:

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

Please try this update then let me if this resolve your problem.

We apologize for any inconvenience this may cause.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on April 04, 2017 at 11:28

Hi Imen thanks for your answer but i have this configuretion code from CubeMX:

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSE;

when i use the  code that you posted it , i see the equal problem

Posted on April 04, 2017 at 12:00

Hi

Buonanno.Antonio

,

In your case, you should removethe oscillator that you don't need

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_***;

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
antonioB
Associate II
Posted on April 04, 2017 at 16:07

thanks, now work only if you select, in  cubemx, the CSS ENABLED in RTC/LCD Source Mux  and  in SYSTEM clock Mux 

Sirma Siang
ST Employee
Posted on April 28, 2017 at 17:49

Hello Antonio,

Great thanks for your inputs.

CubeMX4.20 has a regression in the clock generation code, that pass through all validation tests.

The behave is exactly what you have reported.

This has been corrected in CubeMXv4.20.1.

I advise you to upgrade to that version, and create a new project.

Kind regards

Sirma