cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK Utility Runtime Error

bionix
Associate

Hello,

i am using the ST-LINK Utility 'Serial Wire Viewer' for debbuging three MCU, which are communicating to each other. For a fast opening and exact placement of the windows i use my autohotkey script. Everything work fine, but now i want to set the 'Stimulus port' in my autohotkey scripts. Now i notice, that if i am writing the 'Stimulus port' with the keyvoard into the field i am getting a 'Runtime Error' and the application crashes. It would be glad if it will be possible to write the values or the String 'All' into the field and start the Serial Wire Viewer.

Thanks bionix

0 REPLIES 0