cancel
Showing results for 
Search instead for 
Did you mean: 

ST Link upgrade error

VKoga.1
Associate II

0693W00000GZ9HFQA1.pngWhile I was working to upload firmware to a board STM32CubeIDE refused to upload code until i had updated ST Link from V2.J25.S7 to V2.J39.S7, while I wanted to comply I am getting the following error. Any help is appreciated.

0693W00000GZ9HFQA1.png

19 REPLIES 19
Peter BENSCH
ST Employee

Is the ST-LINK/V2 an original from STMicroelectronics or a clone?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Try a different cable, machine or port​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

robu.in is selling two different ST-LINK/V2: one clone and a genuine one. It should be the right one if it really is the one from your URL, i.e. an ST-LINK/V2 in a white plastic housing with the label ST. The other, cloned ST-LINK/V2 in an aluminum disk shell can be found here.

If it is the latter version, there may well be problems with an upgrade.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I have changed cable & port still facing the same issue,

I got it from the exact URL i posted previously, I will share a photo of it once I get back from work.

So any solution to the problem?​

Do you happen to have a second ST-LINK/V2 to narrow down what/where the problem is?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Uwe Bonnes
Principal III

Show a photo of your device.

I only have a single ST link connected.