2019-10-18 03:10 AM
As this is a prerequisite to installing CubeIDE 1.1.0 one can not install correctly on Mac OS Catalina.
Do we have an ETA for a fix this this problem.
Download site has version 1.1.1. available for download, which is incompatible with Catalina.
/S
2019-11-04 01:02 AM
UP
2019-11-17 12:12 PM
Tried with the recent version, 1.2.0. Yet without any luck!
2019-11-21 08:42 AM
Any reply from ST?
2019-11-30 02:13 AM
Hey ST,
Can we have an ETA for a new release of the STLink server. The STM32CubeIDE is currently only available as version 1.0.2 for MacOS.
And the STLinkServer can not be installed under Catalina.
All that is required here is to compile the App as a 64 bit app instead of the current 32 bit app. Should be doable in a rather short amount of time.
/S
2019-12-10 10:37 PM
Any update on this issue?
Please ST update the driver!
Best regards
2019-12-16 06:45 AM
Up !
An update will be really welcome now.
2019-12-19 08:37 AM
We have been promised a working delivery for the next release of CubeIDE from the team that handles this error and it's set as a blocker. So my guess is that it will be fixed in the next release.
2020-01-01 11:54 AM
Up!