2022-06-21 12:39 AM
Hi community..
I am working with mcu STM32F429 and SRAM with code IS42S16400J .
I have developed a code for init and working with this sram and it was working
void SDRAM_Init(void)
{
volatile uint32_t ptr = 0;
volatile uint32_t i = 0;
/* PB5,PB6 */
GPIOB -> MODER |= ((GPIOB -> MODER) & 0xFFFFC3FF ) | 0x00002800; // AF Function
GPIOB -> OTYPER |= ((GPIOB -> OTYPER) & 0xFFFFFF9F); // Push-Pull
GPIOB -> OSPEEDR |= ((GPIOB -> OSPEEDR) & 0xFFFFC3FF) | 0x00003C00; // Very High Speed
GPIOB -> PUPDR |= ((GPIOB -> PUPDR) & 0xFFFFC3FF); // No Pull-Up
GPIOB -> AFR[0] |= ((GPIOB -> AFR[0]) & 0xF00FFFFF) | 0x0CC00000; //
GPIOB -> AFR[1] |= ((GPIOB -> AFR[1]) & 0xFFFFFFFF) | 0x00000000; //
/* PC0 */
GPIOC -> MODER |= ((GPIOC -> MODER) & 0xFFFFFFFC) | 0x00000002; // AF Function
GPIOC -> OTYPER |= ((GPIOC -> OTYPER) & 0xFFFFFFFE); // Push-Pull
GPIOC -> OSPEEDR |= ((GPIOC -> OSPEEDR) & 0xFFFFFFFC) | 0x00000003; // Very High Speed
GPIOC -> PUPDR |= ((GPIOC -> PUPDR) & 0xFFFFFFFC); // No Pull-Up
GPIOC -> AFR[0] |= ((GPIOC -> AFR[0]) & 0xFFFFFFF0) | 0x0000000C; //
GPIOC -> AFR[1] |= ((GPIOC -> AFR[1]) & 0xFFFFFFFF) | 0x00000000; //
/* PD0,PD1,PD8,PD9,PD10,PD14,PD15 */
GPIOD -> MODER |= ((GPIOD -> MODER) & 0x0FC0FFF0) | 0xA02A000A; // AF Function
GPIOD -> OTYPER |= ((GPIOD -> OTYPER) & 0xFFFF38FC); // Push-Pull
GPIOD -> OSPEEDR |= ((GPIOD -> OSPEEDR) & 0x0FC0FFF0) | 0xF03F000F; // Very High Speed
GPIOD -> PUPDR |= ((GPIOD -> PUPDR) & 0x0FC0FFF0); // No Pull-Up
GPIOD -> AFR[0] |= ((GPIOD -> AFR[0]) & 0xFFFFFF00) | 0x000000CC; //
GPIOD -> AFR[1] |= ((GPIOD -> AFR[1]) & 0x00FFF000) | 0xCC000CCC; //
/* PE0,PE1,PE7,PE8,PE9,PE10,PE11,PE12,PE13,PE14,PE15 */
GPIOE -> MODER |= ((GPIOE -> MODER) & 0x00003FF0) | 0xAAAA800A; // AF Function
GPIOE -> OTYPER |= ((GPIOE -> OTYPER) & 0xFFFF007C); // Push-Pull
GPIOE -> OSPEEDR |= ((GPIOE -> OSPEEDR) & 0x00003FF0) | 0xFFFFC00F; // Very High Speed
GPIOE -> PUPDR |= ((GPIOE -> PUPDR) & 0x00003FF0); // No Pull-Up
GPIOE -> AFR[0] |= ((GPIOE -> AFR[0]) & 0x0FFFFF00) | 0xC00000CC; //
GPIOE -> AFR[1] |= ((GPIOE -> AFR[1]) & 0x00000000) | 0xCCCCCCCC; //
/* PF0,PF1,PF2,PF3,PF4,PF5,PF11,PF12,PF13,PF14,PF15 */
GPIOF -> MODER |= ((GPIOF -> MODER) & 0x003FF000) | 0xAA800AAA; // AF Function
GPIOF -> OTYPER |= ((GPIOF -> OTYPER) & 0xFFFF07C0); // Push-Pull
GPIOF -> OSPEEDR |= ((GPIOF -> OSPEEDR) & 0x003FF000) | 0xFFC00FFF; // Very High Speed
GPIOF -> PUPDR |= ((GPIOF -> PUPDR) & 0x003FF000); // No Pull-Up
GPIOF -> AFR[0] |= ((GPIOF -> AFR[0]) & 0xFF000000) | 0x00CCCCCC; //
GPIOF -> AFR[1] |= ((GPIOF -> AFR[1]) & 0x00000FFF) | 0xCCCCC000; //
/* PG0,PG1,PG4,PG5,PG8,PG15 */
GPIOG -> MODER |= ((GPIOG -> MODER) & 0x3FFCF0F0) | 0x80020A0A; // AF Function
GPIOG -> OTYPER |= ((GPIOG -> OTYPER) & 0xFFFF7ECC); // Push-Pull
GPIOG -> OSPEEDR |= ((GPIOG -> OSPEEDR) & 0x3FFCF0F0) | 0xC0030F0F; // Very High Speed
GPIOG -> PUPDR |= ((GPIOG -> PUPDR) & 0x3FFCF0F0); // No Pull-Up
GPIOG -> AFR[0] |= ((GPIOG -> AFR[0]) & 0xFF00FF00) | 0x00CC00CC; //
GPIOG -> AFR[1] |= ((GPIOG -> AFR[1]) & 0x0FFFFFF0) | 0xC000000C; //
RCC->AHB3ENR |= RCC_AHB3ENR_FMCEN;
// Initialization step 1
FMC_Bank5_6->SDCR[0] = FMC_SDCR1_SDCLK_1 | FMC_SDCR1_RBURST | FMC_SDCR1_RPIPE_1;
FMC_Bank5_6->SDCR[1] = FMC_SDCR1_NR_0 | FMC_SDCR1_MWID_0 | FMC_SDCR1_NB | FMC_SDCR1_CAS;
// Initialization step 2
FMC_Bank5_6->SDTR[0] = TRC(7) | TRP(2);
FMC_Bank5_6->SDTR[1] = TMRD(2) | TXSR(7) | TRAS(4) | TWR(2) | TRCD(2);
// Initialization step 3
while(FMC_Bank5_6->SDSR & FMC_SDSR_BUSY);
FMC_Bank5_6->SDCMR = 1 | FMC_SDCMR_CTB2 | (1 << 5);
// Initialization step 4
for(i = 0; i < 1000000; i++);
// Initialization step 5
while(FMC_Bank5_6->SDSR & FMC_SDSR_BUSY);
FMC_Bank5_6->SDCMR = 2 | FMC_SDCMR_CTB2 | (1 << 5);
// Initialization step 6
while(FMC_Bank5_6->SDSR & FMC_SDSR_BUSY);
FMC_Bank5_6->SDCMR = 3 | FMC_SDCMR_CTB2 | (4 << 5);
// Initialization step 7
while(FMC_Bank5_6->SDSR & FMC_SDSR_BUSY);
FMC_Bank5_6->SDCMR = 4 | FMC_SDCMR_CTB2 | (1 << 5) | (0x231 << 9);
// Initialization step 8
while(FMC_Bank5_6->SDSR & FMC_SDSR_BUSY);
FMC_Bank5_6->SDRTR |= (683 << 1);
while(FMC_Bank5_6->SDSR & FMC_SDSR_BUSY);
// Clear SDRAM
// for(ptr = SDRAM_BASE; ptr < (SDRAM_BASE + SDRAM_SIZE); ptr += 4)
// *((uint32_t *)ptr) = 0x07e007e0;
// for(ptr = SDRAM_BASE; ptr < (SDRAM_BASE + 959); ptr += 4)
// *((uint32_t *)ptr) = 0xFFFFFFFF;
for(ptr = SDRAM_BASE; ptr < (SDRAM_BASE + 0xc7ff); ptr += 4)
*((uint32_t *)ptr) = 0x07e007e0;
for(ptr = SDRAM_BASE + 0xc800; ptr < (SDRAM_BASE + 0x18fff); ptr += 4)
*((uint32_t *)ptr) = 0xf800f800;
for(ptr = SDRAM_BASE + 0x19000; ptr < (SDRAM_BASE + SDRAM_SIZE); ptr += 4)
*((uint32_t *)ptr) = 0x001f001f;
}Then we decided to use an external eeprom for saving some parameters using the following chip AT25640..
I developed the code in a separated project by using the HAL SPI for communicating and saving the parametrs and it was working.
/**
* @brief Function for writing the eeprom
* @param *spi2Handle
* @param *txBuffer
* @param size
* @param addr
* @retval EEPROM_ERROR or EEPROM_OK
*/
uint8_t WriteEEPROM(SPI_HandleTypeDef *spi2Handle, uint8_t *txBuffer, uint16_t size, uint16_t addr)
{
uint8_t addrLow = addr & 0xFF;
uint8_t addrHigh = (addr >> 8);
uint8_t wrenInstruction = WREN_EEPROM;
uint8_t buffer[32] = {WRITE_EEPROM, addrHigh, addrLow};
for(uint8_t i = 0 ; i < size ; i++)
{
buffer[3+i] = txBuffer[i];
}
/*chip select*/
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, RESET);
if(HAL_SPI_Transmit(spi2Handle, &wrenInstruction, 1, TIMEOUT_EEPROM) != HAL_OK)
{
return EEPROM_ERROR;;
}
/*chip select*/
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, SET);
/*delay in ms*/
HAL_Delay(10);
/*chip select*/
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, RESET);
if(HAL_SPI_Transmit(spi2Handle, buffer, (size + 3), TIMEOUT_EEPROM) != HAL_OK)
{
return EEPROM_ERROR;
}
/*delay in ms*/
HAL_Delay(10);
/*chip select*/
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, SET);
return EEPROM_OK;
}When I have imported this function within the project with the init of the sram the sram was not working anymore..
I really i don't understand why an init function is not working by calling the hal spi transmit for writing in eeprom ?
Any idea ?
Do you see something wrong in the init of the code of the sram?
Thanks a lot
2022-06-21 2:07 AM
"the sram was not working anymore"
What, exactly, does that mean?
Are you getting no activity at all on the interface lines?
Is the timing messed-up?
other ... ?
2022-06-21 3:23 AM
It is conncted with a display.. the display it is not working..
Display is blank and it is not possible to see nothing
2022-06-21 3:40 AM
So why do you say that the SRAM is not working?
How do you know it's not just the Display that's stopped working?
Or, perhaps, it's both?
And what does "not working" mean?
Again, have you looked at the interface lines to see what's actually happening in the hardware?
2022-06-21 5:08 AM
Display is blank.. Nothing at all
2022-06-21 5:19 AM
So, again, why do you say that the SRAM is not working?
And, again, have you looked at the interface lines to see what's actually happening in the hardware?
2022-06-21 5:22 AM
It is not clear to me the connection between the sram init and the hal spi transmit.. The display for sure it is using the sram