cancel
Showing results for 
Search instead for 
Did you mean: 

Slow debugging start

ICohe.1
Associate III

Takes about 15 seconds from click on the debug button in CubeIDE to the first break point ( the call to  HAL_Init() ). Custom board, F401RTE, original ST Link V2, using SWD.

Would it be faster using a NUCLEO board ?

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
waclawek.jan
Super User

Subsequent code runs OK?

What's on the board? What is in the startup code? You surely can place a breakpoint at the reset vector's target and then single-step from there, can't you?

I don't use CubeIDE.

JW

Uwe Bonnes
Chief

Does you program sleep for extended periods? When not connecting under reset, debugger needs the CPU awaken to connect

ICohe.1
Associate III

Everything works fine.

The only issue is the time it take from pressing the debug button and until the program is reaching the first line in my program. A call to  HAL_Init()

which is the first line in main(). The board is simple with only eeprom and RTC.

I didn't place any breakpoint it just stop there (on the line with a call to  HAL_Init()) . It is OK to stop there automatically whe I debug. The issue is the time it takes to get there

Here is the printout from the debugger:

 
STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
        Persistent Mode            : Disabled
        Logging Level              : 1
        Listen Port Number         : 61234
        Status Refresh Delay       : 15s
        Verbose Mode               : Disabled
        SWD Debug                  : Enabled
        InitWhile                  : Enabled
 
Waiting for debugger connection...
Debugger connected
      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.4.0                  
      -------------------------------------------------------------------
 
ST-LINK SN  : 54FF72067880565340510267
ST-LINK FW  : V2J36S7
Voltage     : 3.22V
SWD freq    : 4000 KHz
Connect mode: Under Reset
Reset mode  : Hardware reset
Device ID   : 0x433
Device name : STM32F401xD/E
Flash size  : 512 KBytes
Device type : MCU
Device CPU  : Cortex-M4
 
 
Mass erase ... 
 
Mass erase successfully achieved
      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.4.0                  
      -------------------------------------------------------------------
 
ST-LINK SN  : 54FF72067880565340510267
ST-LINK FW  : V2J36S7
Voltage     : 3.22V
SWD freq    : 4000 KHz
Connect mode: Under Reset
Reset mode  : Hardware reset
Device ID   : 0x433
Device name : STM32F401xD/E
Flash size  : 512 KBytes
Device type : MCU
Device CPU  : Cortex-M4
 
 
 
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a17956.srec
  File          : ST-LINK_GDB_server_a17956.srec
  Size          : 25376 Bytes
  Address       : 0x08000000 
 
 
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 1]
Download in Progress:
 
 
File download complete
Time elapsed during download operation: 00:00:01.213
 
 
 
Verifying ...
 
 
 
 
Download verified successfully 
 
 

Erase and download are performed even when no change was made

TDK
Super User

15 seconds seems long. But Eclipse, on which CubeIDE is built, is very slow and clunky in general. Delays of seconds to do operations is not uncommon.

If you feel a post has answered your question, please click "Accept as Solution".
Pavel A.
Super User

> Erase and download are performed even when no change was made

This. Mass erase is slow.

> I didn't place any breakpoint it just stop there (on the line with a call to HAL_Init()) . It is OK to stop there automatically whe I debug.

This is a temporary breakpoint enabled by checkbox "break at main" in the debug config.

If I understand correctly, CubeIDE debugger waits for the first breakpoint hit to fully start debugging.

Until the first breakpoint, it cannot do anything and all debug controls are disabled.

-- pa

ICohe.1
Associate III

Is there a better /faster way to debug both hardwae and software ?

waclawek.jan
Super User

As PavelA said above, avoid mass erase.

I don't know how, I don't use any of the eclipsoids.

JW

TDK
Super User

In my experience with several Eclipse-based IDEs, none of them have performed a full chip erase by default. Seems like yours is both doing a full chip erase, then doing an erase on individual sectors as well.

Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 1]

You'd need to disable the first full chip erase. Not sure how. Look for options in the run configuration settings.

If you feel a post has answered your question, please click "Accept as Solution".
ICohe.1
Associate III

Managed to remove the: monitor flash mass_erase  from the debug configuration.

select Run from the main menu.

then select Debug configuration...

Click on the Startup tab

delete the:

monitor flash mass_erase 

command in the initialization Command box