cancel
Showing results for 
Search instead for 
Did you mean: 

Silkscreen and Schematic Error on X-NUCLEO-GNSS2A1

KMill
Senior

In the schematic for the X-NUCLEO-GNS2A1 it shows the SYS_PSS signal going to J 29

Screenshot 2023-08-03 at 17.34.08.png

J29 shows as being connected to either nothing (PINs 1-2) or "D2D6/PWM" (Pins 2-3)
This is incorrect, the actual circuit is:
PINS 1-2 connect SYS_PPS to D2 on CN5.3 
PINS 2-3 connect SYS_PPS to D6/PWM

That's not so bad, it's just a mis-alignment of the text in the schematic.

However the silk screen on the board at J29 shows that PPS can be conneted to either CN9.3 or CN5.7

Screenshot 2023-08-03 at 17.38.10.png

In fact that should be CN5.3 and CN5.7

 

0 REPLIES 0