2022-12-14 06:58 PM
Dear STMicroelectronics,
The attached file is a product circuit diagram applying STM32F401VET6 as the main CPU.
As for the inquiry, there is a problem that the CPU standard output HIGH signal drops to LOW signal at a specific PORT when performing ESD test.
The specific PORT is as follows.
=>PB2,PB3,PB4,PB5,PB6,PB7,PB8,PB9,PB10,PB12,PB13,PB14,PB15,PC0,PC1,PC2,PC3,PC4,PC5,PC6,PC8,PC9,PC10,PC11. PC12, PC13
=> A specific PORT is the input signal (Base) of the PNP Transitor-applied switching circuit, and functions to turn on (High) and turn off (Low) the LED.
Please review the attached circuit diagram and PCB.
Thank you.
Solved! Go to Solution.
2022-12-16 04:02 AM
Hi again,
first of all, the ESD level of STM32F401xE alone for IEC 61000-4-2 is 2B according to datasheet, which is under 1kV (see AN1709).
To improve this:
BR,
Jaroslav
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-15 12:44 AM
Hi @Inho Jeon,
could you please clarify what kind of ESD test is failing? Is it IEC 61000-4-2, or other? Also at which ESD level does this behavior occur?
BR,
Jaroslav
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-15 11:31 PM
Dear Jaroslav,
Yes, It is failed at contact -4KV of ESD on IEC 61000-4-2.
Thank you.
Best Regards,
Inho Jeon
2022-12-16 03:41 AM
Where's the contact happening?
I haven't seen any protection diodes / varistors / whatever, so you purely rely on the ICs' ESD capabilities?
Problem with that: you cannot control the (over-) current flow.
Think like: where's the current flowing? Probably within / through the device then through system GND. And then you're probably f*****. ;)
That's why external protection "devices" make sense, and best practice to connect their GND not "somewhere" to PCB GND, ideally to some other low impedance path, e.g. metal case.
2022-12-16 04:02 AM
Hi again,
first of all, the ESD level of STM32F401xE alone for IEC 61000-4-2 is 2B according to datasheet, which is under 1kV (see AN1709).
To improve this:
BR,
Jaroslav
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.