cancel
Showing results for 
Search instead for 
Did you mean: 

Recommendation for STM32F4 MCU with Multiple UARTs, Quad SPI, and 100-120 MHz Frequency

parth4
Associate II

Hello ST Community,

I am looking for an STM32F4 series microcontroller that meets the following requirements:

:small_blue_diamond: Microcontroller Requirements:
:white_heavy_check_mark: More than 2 UART ports
:white_heavy_check_mark: Quad SPI support
:white_heavy_check_mark: Operating frequency: 100-120 MHz
:white_heavy_check_mark: Preferred package: TQFP/LQFP, but open to other suggestions

Since this MCU will be used in an embedded system, power efficiency and peripheral availability are key considerations.

3 REPLIES 3
Peter BENSCH
ST Employee

Have you ever filtered your selection on the websites of the STM32F4?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Mike_ST
ST Employee

Hello,

For power efficiency as you mentionned, you might want to look at a newer STM32 range as the F4 family is a bit old.

For example STM32U5 or STM32L4+.