2024-09-09 07:41 AM
Hello, I am working on a project which receives an analog square signal and the idea is to read the ADC values, and try to recreate (based on the ADC values) the square signal inside the microcontroller, but not to output in another pin, instead to detect/understand (with a threshold) what ADC values refer to the low and high positions of the square wave being feed and decode a message if any. To note, the square wave low means 0 and high means 1.
I have tried with single (stm32f4 series) and double (stm32l4 series) ADC, using DMA for both cases, but in both scenarios I get ADC values I can't make sense to recreate the frequency of the input signal and recreate any encoded message. I am able to identify minimum and maximum values, but the result is a wave which doesn't get similar to the one feed as input. I am attaching readings values from the ADC.
Has someone tried to do this? I feel I am missing something, maybe the use of a clock or my ADC configuration is wrong, the sampling. My last attempt is with a stm32l4 series microcontroller, DMA and using FreeRTOS.
This is the configuration code to configuring two ADC to work together:
/**
* @brief ADC1 Initialization Function
* @PAram None
* @retval None
*/
static void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
ADC_MultiModeTypeDef multimode = {0};
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Common config
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.NbrOfConversion = 1;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = ENABLE;
hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
hadc1.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure the ADC multi-mode
*/
multimode.Mode = ADC_DUALMODE_INTERL;
multimode.DMAAccessMode = ADC_DMAACCESSMODE_12_10_BITS;
multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_5CYCLES;
if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_247CYCLES_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC1_Init 2 */
/* USER CODE END ADC1_Init 2 */
}
/**
* @brief ADC2 Initialization Function
* @PAram None
* @retval None
*/
static void MX_ADC2_Init(void)
{
/* USER CODE BEGIN ADC2_Init 0 */
/* USER CODE END ADC2_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC2_Init 1 */
/* USER CODE END ADC2_Init 1 */
/** Common config
*/
hadc2.Instance = ADC2;
hadc2.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc2.Init.Resolution = ADC_RESOLUTION_12B;
hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc2.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc2.Init.LowPowerAutoWait = DISABLE;
hadc2.Init.ContinuousConvMode = ENABLE;
hadc2.Init.NbrOfConversion = 1;
hadc2.Init.DiscontinuousConvMode = DISABLE;
hadc2.Init.DMAContinuousRequests = ENABLE;
hadc2.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc2.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc2) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_247CYCLES_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC2_Init 2 */
/* USER CODE END ADC2_Init 2 */
}
The callback functions:
/**
* @brief Conversion complete callback in non blocking mode
* @PAram AdcHandle : ADC handle
* @note This example shows a simple way to report end of conversion
* and get conversion result. You can add your own implementation.
* @note When ADC_TRIGGER_FROM_TIMER is disabled, conversions are software-triggered
* and are too fast for DMA post-processing. Therefore, to reduce the computational
* load, the output buffer filled up by the DMA is post-processed only when
* ADC_TRIGGER_FROM_TIMER is enabled.
* @retval None
*/
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
uint32_t tmp_index = 0;
/* For the purpose of this example, dispatch dual conversion values */
/* into 2 arrays corresponding to each ADC conversion values. */
for (tmp_index = (ADC_BUFFER_SIZE/2); tmp_index < ADC_BUFFER_SIZE; tmp_index++)
{
aADCxConvertedValues[tmp_index] = (uint16_t) GET_ADC1_RESULT(aADCDualConvertedValues[tmp_index]);
aADCyConvertedValues[tmp_index] = (uint16_t) GET_ADC2_RESULT(aADCDualConvertedValues[tmp_index]);
}
/* Reset variable to report DMA transfer status to main program */
ubADCDualConversionComplete = SET;
}
/**
* @brief Conversion DMA half-transfer callback in non blocking mode
* @PAram hadc: ADC handle
* @note When ADC_TRIGGER_FROM_TIMER is disabled, conversions are software-triggered
* and are too fast for DMA post-processing. Therefore, to reduce the computational
* load, the output buffer filled up by the DMA is post-processed only when
* ADC_TRIGGER_FROM_TIMER is enabled.
* @retval None
*/
void HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef* hadc)
{
uint32_t tmp_index = 0;
/* For the purpose of this example, dispatch dual conversion values */
/* into 2 arrays corresponding to each ADC conversion values. */
for (tmp_index = 0; tmp_index < (ADC_BUFFER_SIZE/2); tmp_index++)
{
aADCxConvertedValues[tmp_index] = (uint16_t) GET_ADC1_RESULT(aADCDualConvertedValues[tmp_index]);
aADCyConvertedValues[tmp_index] = (uint16_t) GET_ADC2_RESULT(aADCDualConvertedValues[tmp_index]);
}
/* Reset variable to report DMA transfer status to main program */
ubADCDualConversionComplete = RESET;
}
The FreeRTOS task:
/* USER CODE BEGIN 5 */
/* Infinite loop */
for(;;)
{
if (ubADCDualConversionComplete == RESET) {
for (uint32_t i = 0; i < 128; i++)
{
// Average just to test if I get a better reconstruction
uint16_t averageRead = (aADCxConvertedValues[i] + aADCyConvertedValues[i]) / 2;
printf("%u\r\n", averageRead);
if (averageRead >= 500) {
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_2, GPIO_PIN_SET);
} else {
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_2, GPIO_PIN_RESET);
}
}
}
}
// In case we accidentally exit from task loop
osThreadTerminate(NULL);
/* USER CODE END 5 */
2024-09-09 08:07 AM
Hello and welcome to the community,
@gioyik wrote:
the square wave low means 0 and high means 1.
What do you mean by 0 and 1? voltage levels 0 and 1V?
@gioyik wrote:
I get ADC values I can't make sense to recreate the frequency of the input signal and recreate any encoded message.
Your samples have two values ~1490 and ~149. So the square is there.
But what is the frequency of your signal input and what is the sampling frequency of the ADC?
The Nyquist-Shannon sampling theorem states that to accurately reconstruct a signal, it must be sampled at a rate at least twice its highest frequency.