2025-02-01 6:47 PM
I am doing a datalogger application with a custom piece of hardware using STM32 and FileX middleware. While datalogging, it occassionally experiences a spike in write and flush times that seems to be random to me. So I tried to make a simple application just to test it.
The setup: The custom board uses STM32H563 MCU directly connected to the SD card slot hardware component. I generated my code using STM32CubeMX with FileX in standalone mode. So I am not using LevelX or ThreadX (from Azure RTOS). The SDMMC peripheral has a clock speed of 25MHz, with 0 SDMMC clock divide factor. This gives me the maximum SD default speed according to the reference manual. The SD cards used are FAT32 with 4096KB sector size.
For debugging and testing purposes, I am continuously logging an array of 32768 bytes that is in the program. I have given the media file 102400 bytes that is aligned to 32 bytes. The code is simple. With the media and file open, the code writes the 32KB of data and immediately flush the data repeatedly. I time the write and flush operations with a timer and log it into the array that I can see when I pause the debugging. For all tests, I run them in debug mode with a ST link V2 clone.
What I found and thought so far: The write and flush times are consistent. Until randomly, the write and flush time spikes up. As an example, it normally takes 40ms per write and flush, and when it spikes, it takes 800ms instead.
I have done the test with and without formatting the SD card and it seems the time spikes occur after a similar number of writes, but never really the same.
The frequency of this happening seems to be significantly higher on an unbranded SD card. On branded SD cards, it happens rarely, like once every 3000+ writes. The size of the spike also varies, it could be 200ms to 800ms.
The datalogger has suffcient writing speed for my application. However, when a spike in time like this occurs, my buffers may overflow. I would like to understand what are these spikes in time, and if there is any way to avoid it other than to increase my buffers.
My questions are: Could they be caused by the attached debugger? Is this the result of some garbage collection, SD FAT table udpates or bad sectors? Is this spike in time similar for other applications? I do not have any other possible datalogger in my possession right now.
Solved! Go to Solution.
2025-02-02 3:36 AM - edited 2025-02-02 3:37 AM
SD cards need some time, to respond on a command.
Ok, this is about 0,5...1ms on good , new cards. But after some use...times go up...see here a speed check:
on 2 y used Intenso 16GB card:
From general sd-card specification you have to deal with up to 100ms delay ! (over 300ms delay = defective).
"Cheap" cards (from China...) might run very good, but also very bad , is just rolling the dice .
So your program needs some buffering, at least to deal with 100ms (perfect: 300ms) "no reaction time" on R or W to card.
The debugger or 1 or 4-bit mode is not the basic problem, there is no other solution than to deal with the possible random delays. And try testing it with some used, old, cheap card - if it works with these, your program will work.
2025-02-02 3:36 AM - edited 2025-02-02 3:37 AM
SD cards need some time, to respond on a command.
Ok, this is about 0,5...1ms on good , new cards. But after some use...times go up...see here a speed check:
on 2 y used Intenso 16GB card:
From general sd-card specification you have to deal with up to 100ms delay ! (over 300ms delay = defective).
"Cheap" cards (from China...) might run very good, but also very bad , is just rolling the dice .
So your program needs some buffering, at least to deal with 100ms (perfect: 300ms) "no reaction time" on R or W to card.
The debugger or 1 or 4-bit mode is not the basic problem, there is no other solution than to deal with the possible random delays. And try testing it with some used, old, cheap card - if it works with these, your program will work.
2025-02-03 7:59 PM
Hi Ascha. Thank you for your reply! I now understand that the SD card takes time to respond. Can I ask further, if this delay is caused by internal processes in the SD card or that it just needs more time to access an area in memory? e.g. updating a FAT table.
2025-02-04 12:09 AM
Hi,
afaik its the management on the card; (we cannot change, we even dont know exactly); you know they do internal management of bad blocks, suspicious blocks (that need error correction already) and always wear leveling , that moves blocks of data to new or less used memory area, what needs some extra time at write access. And more and more error correction or multible reads on same sector will need time.
So all cards will get more or less "slower" , when old or heavy used. Cheap cards more, expensive "special" cards less.