cancel
Showing results for 
Search instead for 
Did you mean: 

"no STM32 target found" with ST-LINK V2 ISOL

Kunal
Associate II

I purchased a new ST-LINK V2 ISOL debugger but whenever i connect it to my custom STSPIN32F0 board using SWD protocol (VCC, SDA,SCLK, GND), its showing no STM32 target found and error showing target voltage is too low but 3.3 V showing on the VCC pin.

2 REPLIES 2

How is the board powered?

Is it otherwise functional?

Show the salient portion of the schematic.

Make sure the ST-LINK/V2 has current firmware.

​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Kunal
Associate II

Please find my replies inline:

How is the board powered?

The board is powered through ac (220-240 V) which then goes through a full bridge and then through a LDO to supply 3.3 V on MCU (3.3 V is detected).

Is it otherwise functional?

Yes it was functional with earlier boards.

I cross checked the connections of the programming pins, they were soldered poorly. By again doing so, the connections became proper and the programming is functional now. Thanks for your valuable feedback.