2024-06-10 5:40 AM - last edited on 2024-06-10 5:51 AM by Tesla DeLorean
Hi, Im using NUCLEO-H753ZI board and i want to send raw data to computer terminal. i tried to by using USART1. according to the schematics i can send data via USRAT1 through the USB power connection and it not working. i also tried to use USB_DEVICE to send the data but it fails again.
in my last project i have used NUCLEO-U575ZI-Q and i send the data with USART1 and there were no problem at all.
can someone can help?
Solved! Go to Solution.
2024-06-10 5:49 AM - edited 2024-06-10 5:49 AM
Not all NUCLEO boards have the same USART connected to the ST-LINK for a Virtual COM Port VCP, e.g. on the NUCLEO-H753ZI it is USART3, as can be seen from the schematics.
Hope that helps?
Regards
/Peter
2024-06-10 5:49 AM - edited 2024-06-10 5:49 AM
Not all NUCLEO boards have the same USART connected to the ST-LINK for a Virtual COM Port VCP, e.g. on the NUCLEO-H753ZI it is USART3, as can be seen from the schematics.
Hope that helps?
Regards
/Peter
2024-06-10 5:50 AM
Unfortunately "not working" is not a particularly helpful description.
The NUCLEO-H753ZI should have a ST-LINK/V3 with a VCP. Not sure of the band-width limit there, but I'd imagine it's quite high. Does it work at lower speeds?
Doesn't the VCP use USART3 PD8 / PD9 ?
USB fails? Fails HOW?
Anticipate you might have to debug your situation.
2024-06-16 12:11 AM
Thank you for your answer,
i saw to that the USART3 is connected to VCP and i start the transmission with:
HAL_UART_Transmit(&huart3, (uint8_t *)txBuf, len, HAL_MAX_DELAY);
when im in debug mode and i reach to the transmission command the command seems executed just fine but there is no output on the computer terminal.
my configuration is USAT3, Mode >> Asynchronous, Baud Rate >> 115200.
The remaining configurations were not changed.
I have tried to change the baud rate to 9600 and still the same result.
hope i manage to explain more efficiently the problem