2022-11-15 11:11 AM
Debug project with external loader
Hi all,
I have a project with an external loader and I didn't succeed to enter to debug and download the hex (sometimes is and sometimes it is not it didn't consistency
i didn't understand if it's the st programmer or
see log :
STMicroelectronics ST-LINK GDB server. Version 7.0.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\TFS\Software\Projects\RK\source_code\release\code_2024\controlller\1\rks_controller\debug_new\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61244
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
InitWhile : Enabled
COM frequency = 4000 kHz
Target connection mode: Under reset
Reading ROM table for AP 0 @0xe00fdfd0
Hardware watchpoint supported by the target
ST-LINK Firmware version : V2J40S7
Device ID: 0x452
PC: 0x800b380
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.22 V
ST-LINK device status: HALT_MODE
Run external memory initializer
ST-LINK device initialization OK
Stm32Device, pollAndNotify running...
SwvSrv state change: 0 -> 1
Waiting for connection on port 61245...
Waiting for debugger connection...
Waiting for connection on port 61244...
Accepted connection on port 61244...
Debugger connected
Waiting for debugger connection...
Waiting for connection on port 61244...
GDB session thread running
GdbSessionManager, session started: 1
Warning: Ignoring a '-' sent by client....
Stm32Device, closeDevice() entry
GDB session, device event: 5
Stm32Device, pollAndNotify stopped
Stm32Device, closeDevice() exit
------ Switching to STM32CubeProgrammer -----
-------------------------------------------------------------------
STM32CubeProgrammer v2.8.0
-------------------------------------------------------------------
Log output file: C:\Users\nbitan\AppData\Local\Temp\STM32CubeProgrammer_a25876.log
Warning: Wrong connect parameter: speed=fast
ST-Link Server is running on port : 7184
ST-LINK SN : 50FF6F067788545406291867
ST-LINK FW : V2J40S7
Board : --
Voltage : 3.22V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x452
Revision ID : Rev A
Device name : STM32F72x/STM32F73x
Flash size : 64 KBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x__
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a25876.srec
File : ST-LINK_GDB_server_a25876.srec
Size : 594368 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing memory corresponding to segment 1:
Erasing external memory sectors [0 8]
Download in Progress:
�������������������������������������������������� 0%
��������������������� 43%
Error: failed to download Segment[0]
Error: failed to download the File
------ Switching context -----
COM frequency = 4000 kHz
Target connection mode: Under reset
Reading ROM table for AP 0 @0xe00fdfd0
Hardware watchpoint supported by the target
ST-LINK Firmware version : V2J40S7
Device ID: 0x452
PC: 0x800b380
ST-LINK detects target voltage = 3.22 V
ST-LINK device status: HALT_MODE
Run external memory initializer
GDB session, device event: 3
GDB session, device event: 1
ST-LINK device status: RUN_MODE
GDB session, device event: 4
GDB session, device event: 4
GDB session, device event: 6
Stm32Device, pollAndNotify running...
ST-LINK device status: HALT_MODE
GDB session, device event: 0
GDB session, device event: 3
GDB session, device event: 1
GDB session, device event: 0
NVIC_DFSR_REG = 0x0000000B
GDB session, device event: 3
GDB session, device event: 1
ST-LINK device status: RUN_MODE
2022-11-15 12:48 PM
What you've provided here isn't particularly enlightening.
Is this a custom board, using a custom loader?
What STM32, pins and memory chip?
Is this something where you've previously tested the code?
Best to debug the BSP code outside of the loader first.
Use current version of the STM32 Cube Programmer, use higher Verbose level to understand the programmer's perspective.
Instrument your loader to use resources on your board, like a UART, to provide details from the loader's perspective.
2022-11-15 1:40 PM
so the story is that I have 2 projects
Both of them work great we succeed to burn and operate
I use cube ide 10
in the project -STM32H750+GD25Q127CSIGR external flash -custom board, custom loader
in the start, I have a problem with the download but after replacing the cube programmer from version 2.11 to 2.8 it all work very (succeed in downloading and debugging well)
with the st-link tool connected to SWD
I face issues some of the time it's successful to download and most of the time not and not enter to debug
what do you mean by -use higher Verbose level
any advice?
2022-11-17 6:00 AM
any answer?
2022-11-17 10:24 AM
Sorry lot of specific stuff that I don't have, on a project that's not mine..
Both the GUI and CLI versions of STM32 Cube Programmer have methods to select the "Verbosity" of the logging output. These might provide some insight into what interactions are failing. Things like registers, timing of the interactions, timeouts, etc.
If you want insight into what the loader sees from inside the MCU you'll have to add instrumentation to report via a serial port that's available on your board.
2022-11-22 4:39 AM
Hi
I am working from the cubeIDE can you please be more specific on how to active the verbose mode in the debug? i try to read about that and didn't find info