2023-06-02 6:51 PM
I'm currently working on a project involving a NUCLEO-H743ZI2 board.
I want to know if it's possible to power the board with User USB instead of ST-Link USB.
Or if it's possible to transfer data using ST-Link USB and use User USB for debugging.
Thank you in advance!
Solved! Go to Solution.
2023-06-05 12:48 AM
Frankly I've never tried this)) A common ground is needed. But there's the 5V power.
2023-06-05 1:07 AM
It's almost a joke... I don't know how the other side will react, especially with a USB C.
2023-06-11 3:16 PM - edited 2023-11-20 4:05 AM
@pavel A. @Nikita91 @FLeon.4 @Rodo
I found the board NUCLEO-H743ZI2 can be powered by the user usb automatically.
First, I need to connect both ST-Link USB and User USB to two USB ports.
Then, I can just unplug the ST-Link USB and the board is still running.
Not sure why.
I also attached a image below. As you can see, the LED lights are on and ST-Link usb(black) is unplugged
The trick is let ST-Link USB power the board first then switch to User USB by unpluging the ST-Link USB.
I'm not sure this functionality is mentioned on the user manual.
Is there a way to make the board boot up from User USB?
Thanks!
2023-06-11 4:14 PM
> Is there a way to make the board boot up from User USB?
Now we are back to square one.
2023-06-12 7:51 PM
Hello again,
What do you mean by "square one"?
2023-06-13 1:16 AM
Return to the question at the beginning of this post.
The 1st step of the game...