cancel
Showing results for 
Search instead for 
Did you mean: 

Overcurrent Issue when connecting a display

Ridddddd
Associate

Hello, I am currently working with a STM32 development board that I am using to power (and code) a PCB that has an stm32 chip. So far, it has been working properly but I recently connected the PCB to a display (Newhaven display: LINK) and now the "overcurrent" LED is lighting up on the STM32 development board. Once I disconnect the display, it goes back to normal. Please refer to the pictures attached below. Additionally, please note that the display doesn't turn on and idk if it is due to the "overcurrent" issue. I am using a FFC Jumper cable and I'm pretty sure that it is connected properly. I am sending 3.3V to the PCB which should be fine.

Please help me as I am really confused.

 

With the display connected:

20250414_153203.jpg

Without the display:

20250414_153117.jpg

The display:

20250414_153130.jpg

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
mÆŽALLEm
ST Employee

Hello @Ridddddd and welcome to the ST community,

Most probably the display you are adding to the board pulls more current that the board can generate especially due to the backlight of the LCD.

I propose to power supply the LCD with an external power source and ensure the common GND.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
mÆŽALLEm
ST Employee

Hello @Ridddddd and welcome to the ST community,

Most probably the display you are adding to the board pulls more current that the board can generate especially due to the backlight of the LCD.

I propose to power supply the LCD with an external power source and ensure the common GND.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
EZHON.1
ST Employee

it seems you are using the STLINK-V2-1, the current ask from the USB is 100mA at the beginning of the STLINK starting.  when you add the LCD, could you check the current consumption from LCD. if less than 500mA from LCD, you can use a pin to control LCD backlight or whole power to avoid the STLINK enumeration step.