2024-08-07 7:06 AM - last edited on 2024-08-07 7:24 AM by STTwo-32
Hi! Im looking for a microcontroller with a lot of gpio. I have looked into NUCLEO-H755ZI-Q. As I understand it shall provide me with 144 gpio but im not sure if I need some header for this to happen? I have read about ST Zio and morpho connectivity but not sure what exactly that means? How can I access all gpio? What exactly do I need or do NUCLEO-H755ZI-Q provide all these outputs out of the box?
Are there any microcontroller with even more gpio?
2024-08-07 7:12 AM - edited 2024-08-07 7:19 AM
@pero wrote:Hi! Im looking for a microcontroller with a lot of gpio. I have looked into NUCLEO-H755ZI-Q.
The NUCLEO-H755ZI-Q is a board - not a microcontroller.
Do you actually mean a board, or a microcontroller (ie, just the chip itself - for incorporating into your own design)?
EDIT (sorry - posted too soon):
@pero wrote:As I understand it shall provide me with 144 gpio
It provides a total of 144 pins - they may or may not all be available for use as GPIO
@pero wrote:I have read about ST Zio and morpho connectivity but not sure what exactly that means?
They are explained in the User Manual:
@pero wrote:How can I access all gpio?
The connector pinouts are all documented in the User Manual.
See also the schematics.
@pero wrote:Are there any microcontroller with even more gpio?
Again, do you mean boards, or do you mean microcontrollers ?
2024-08-07 7:17 AM
Sorry. I meant the boar
2024-08-07 7:22 AM
I accidentally posted to soon - see the edit for more details on the board ...
2024-08-07 7:34 AM - edited 2024-08-07 7:35 AM
@Andrew Neil It provides a total of 144pins - they may or may not all be available for use as GPIO
But can I just access these the same way as on arduino or esp32? For example just solder a female header on st expansion header and use it as normal on esp32 or arduino? How many are actually available and not reserved for other stuff?
2024-08-07 8:05 AM
Again, see the User manual: