2020-09-27 7:37 AM
Hi,
I am using STM32 controller (STM32L475VC) for our project. I am getting error as "NO TARGET FOUND" when
I have done following steps to erase & program the controller
Kindly, provide support for this issue.
Regards,
Sanjay
2020-09-27 9:07 AM
Has it every worked? custom board?
Pins not wired properly, buffers on ST-LINK/V2 not powered properly, see pin 1/2
Conflicting with other devices connected to SWDIO/SWCLK
2020-09-27 9:47 PM
Yes it was working Custom board. Pins are wired properly. SWDIO/SWCLK pin are not conflicting with others