2021-01-24 2:31 PM
I have an stm32f401vc discovery card, I can't download and debug the code you can find the error in this picture
 
when I connected the card to my pc here is what I found in the Device manager
I worked on this card for a long time and this is the first time that I find this error
the most shocking thing that the serial port works
2021-01-24 5:43 PM
Hello
it seems that the driver is not installed or installed incorrectly. VCPort(com8) is not stlink for debug. Only mini USB side of the board must be connected to PC.
Download drivers from here ..
2021-01-25 2:30 AM
I installed the driver
maybe the cable is damaged no ?