cancel
Showing results for 
Search instead for 
Did you mean: 

''No ST-LINK detected'' when connecting with stm32f401 board

Sdrid.1
Associate II

I have an stm32f401vc discovery card, I can't download and debug the code you can find the error in this picture

0693W000007CSJSQA4.png 

when I connected the card to my pc here is what I found in the Device manager

0693W000007CSJXQA4.pngI worked on this card for a long time and this is the first time that I find this error

the most shocking thing that the serial port works

0693W000007CSJNQA4.png

2 REPLIES 2

Hello

it seems that the driver is not installed or installed incorrectly. VCPort(com8) is not stlink for debug. Only mini USB side of the board must be connected to PC.

Download drivers from here ..

Sdrid.1
Associate II

I installed the driver

maybe the cable is damaged no ?