2023-05-17 05:37 AM
I have no previous experience on ST tools. I have a brand new STLINK-V3MiniE. I installed the driver and trying the STM32CubeProgrammer as the first step to verify target connection. I get no response whatsoever from the device, with or without target Vcc present (+3.3V). No lights and nothing on the PC side, except for an error message about unregonized USB device. The programmer doesn't see it either.
What is the expected behaviour and am I right to assume that I got a faulty unit and need to buy another?
2023-05-17 06:57 AM - edited 2023-11-20 05:13 AM
on PC - which system ? Win x , Linux .. ?
on Win hear USB connection, ding-****, see in STMCubeProgrammer -> refresh :
and in hardware manager on windows ->
and on stlink-V3 red LED on - otherwise take another cable and USB port...
2023-05-17 08:19 AM
Sorry, WIndows 10. And no, no sound, nothing on device manager, no LED. I guess I god a dud. Ok, no big deal, those are practically free.
2023-05-17 08:38 AM
on win10 (other PC from co-worker ) "nothing" happens , no error, no sound.
but no LED -> no power at all ! -> take another cable and other USB port... and check !
2023-05-17 08:43 AM
STLink SW update notification kicks in CubeIDE (for example).
2023-05-17 09:01 AM
Just a regular PC. STLink is connected to target with 10cm wires. I even tried with just the gnd and Vcc to ensure, that wrong target connections are out of play. The port and cable are ok - at least giving power to a phone.
2023-05-17 08:52 PM
I was wondering if this is a USB-C specific cable incompatibility. Can you try with an adapter which disable any USB power delivery feature ?