2021-07-29 6:49 AM
I've updated several Nucleo-H743 with the ST-LINK update that comes with CubeIDE 1.7.0 for Windows. This updater allows to choose mode without a USB drive and annoying popup on connection.
The debugger of CubeIDE 1.7.0 works well with this firmware.
However co-workers complain that CubeProgrammer and maybe also CubeIDE 1.6.x fail to recognized the ST-LINK.
The old good ST-LINK utility works with this update just fine.
--pa
2021-07-29 9:01 AM
Could they just update the ST-LINK related EXE/DLL/SYS files to use a consistent pod/drivers?
Sometimes with Adobe FLASH, the winning move is not to play..