2022-04-30 7:52 AM
A new batch of electronic board mount an STM32F05R8T6
AA170 9U
TWN AA 131 marked.
All of this devices don't start up LSE clock.
The code is the same for about five years and makes the LSE clock start up till this days correctly. The initialization was made using example code bundled with discovery stm32F051.
I create with CubeIDE Version: 1.9.0 a minimal setup (CubeMX) for initializa internal RC but the code hangs on
while(__HAL_RCC_GET_FLAG(RCC_FLAG_LSERDY) == RESET)
{
if((HAL_GetTick() - tickstart ) > RCC_LSE_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}The quartz is the same sice five years and i try to modify the capacitor from 15nF to 6,8nF with no success.
Same board with STM32F05R8T6
GQ272 9U
CHN GQ 944 marked
run perfectly.
Any ideas?
Thanks
Fabio
Solved! Go to Solution.
2022-05-03 12:32 AM
Have you tried any of what I wrote above, e.g. playing with LSEDRV?
JW
2022-05-03 11:13 AM
Yes changing LSEDRV nothing happen.
And untill this batch of micro we made about one thousand of board with LSE Ok...
2022-05-03 11:55 AM
2022-05-03 11:01 PM
Yes nothing change...
Thing change using older batch STM32F051...
2022-05-04 1:55 AM
At this point you may want to contact ST directly, through FAE or the web contact form.
JW
2022-05-04 7:25 AM
Hi @passafabio2 ,
As suggested by @Community member , I'm checking internally if there is any noted change regarding LSE as I'm not aware of any update.
In such case, a failure analysis request (FAR) will be required and needs to be initiated by your FAE.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-05-04 10:38 AM
Yes nothing change.
2022-05-04 1:56 PM
Hi @Amel NASRI
I'd assume there's a new RM0091 somewhere covering the new ICs, the one publicly available is over 5 years old, and clearly not up to date.
Even if it is a new/duplicate mask-set for a new fab.
"9U" is the TSMC USA Fab 11
"98" is the TSMC Taiwan Fab 8
And in 2019 some was moved to "9C" TSMC Singapore pursuant to PCN MDG/19/10803
2022-05-04 2:11 PM
Any observation in the Markings or IDCODE for the older working ones?
This might help narrow down the production date / window, and a source for the wafers.
Other things that might change over time is the System Memory / Boot Loader version, although I don't perceive that as impacting LSE in any way.
2022-05-04 2:20 PM
The errata seems less stale, but only covers the 0x2000 device
But nothing about LSE