2022-04-30 7:52 AM
A new batch of electronic board mount an STM32F05R8T6
AA170 9U
TWN AA 131 marked.
All of this devices don't start up LSE clock.
The code is the same for about five years and makes the LSE clock start up till this days correctly. The initialization was made using example code bundled with discovery stm32F051.
I create with CubeIDE Version: 1.9.0 a minimal setup (CubeMX) for initializa internal RC but the code hangs on
while(__HAL_RCC_GET_FLAG(RCC_FLAG_LSERDY) == RESET)
{
if((HAL_GetTick() - tickstart ) > RCC_LSE_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}The quartz is the same sice five years and i try to modify the capacitor from 15nF to 6,8nF with no success.
Same board with STM32F05R8T6
GQ272 9U
CHN GQ 944 marked
run perfectly.
Any ideas?
Thanks
Fabio
Solved! Go to Solution.
2022-05-16 7:48 AM
Hello,
The ES0202 is up to date and describing last silicon on market. No new silicon developed for this line since 2014. Your 2 products are both dated from 2021 and 2019 by decoding your date code. So if you compare both IDCODE I expect you read same value, so same silicon.
The production plant changed as stated in a previous posts, but this is not documented in either RM or ES (besides change of revision on top right corner of package being B,1 or 2) or your packaging location, which neither should lead to LSE being not functional.
We could imagine very small drift in process or electrical charac due to those changes, but it seems impossible that a full batch would be defective.
As suggested by Jan may you check this:
"populate a known good tested working board (such as Nucleo or Disco, or maybe even an older device of yours) with the new 'F051."
In case of defectivity, it should go to (FAR) initiated by your local FAE.
Regarding the LSE itself, in a failed startup state, what voltage do you see on OSC32_IN and OSC32_OUT?
Thank you and regards,
Antoine
2022-05-25 8:45 AM
"populate a known good tested working board (such as Nucleo or Disco, or maybe even an older device of yours) with the new 'F051."
As described before i made this. In a first post I wrote:
Same board with STM32F05R8T6 -> "old device" remains from precedent batch
GQ272 9U
CHN GQ 944 marked
run perfectly.
STM32F05R8T6 has a Discovery board, but the 32Khz768 is not mounted from st.
2022-05-25 10:27 AM
Right, but I think Jan's point would be to populate parts onto the board. Presumably with parts from ST's BOM, testing the LSE examples, and then perhaps with your crystal.
You look to have gone through a lot of diagnostic steps, if you're confident there's an issue here, you need to push it in via usual support/engineering channels.
Did you initiate a Failure Analysis Report with your local FAE or distributor? I think you're probably seeing a real issue, and that would be the way to advance it, as I don't think you're going to get much further on this thread.
Also pull whatever production/trace codes are on the part reels, and get that to an FAE
2022-05-25 1:10 PM
My point with "known good" board was that maybe your boards - both old and new - have something which makes them marginal in a way that some parts which came out "slightly better than average" work in both, and the parts which came out "slightly worse but still conforming to specs" don't.
And yes, I meant it as Clive Tesla DeLorean said - use your crystal, and if still no joy, try to use ST's crystal.
Also, post here a minimal but complete compilable code you use for testing, for us to review.
Also, answer Antoine's question.
As both Antoine and Clive said above, at this point you have to talk to ST directly. Note, that we are mere users here, and those who are tagged as ST Employees don't necessarily work as support.
JW
2022-06-01 11:39 PM
"Did you initiate a Failure Analysis Report with your local FAE or distributor"...Done by our assembler mfg to their distributor more a month ago. Still waiting...
2023-10-09 8:14 AM
The problem seem the poor cleaning made by manufacturer when they find a Sn join between the 32Khz768 quartz pins. Fixing the unwanted join with soldering wire they don't clean well the water based flux and in some occasions made a lower impededence which makes quartz unable to run. The quartz with soldered join is covered with a 16X2 lcd display then detected dirty pin wasn't immediate.
The first batch of stm32f051RBT8 was more strong in oscillating.
Fabio