cancel
Showing results for 
Search instead for 
Did you mean: 

Need schematic of STM2H743ZI2.

PREDATOR
Associate II

Only schematic of STM32H743ZI is available, not for STM2H743ZI2, how can I get schematic diagram of STM2H743ZI2 ?

1 ACCEPTED SOLUTION

Accepted Solutions
Nikita91
Lead II

Strange...

Schematics 1.1 is MB1137 rev B-01 from 2015, with STLINK V2-1

Schematics MB1364-H743ZI-C01 Schematics 1.0 is MB1364 rev C-01 from 2018, with STLINK V3

View solution in original post

4 REPLIES 4
Imen.D
ST Employee

Hello @PREDATOR​ ,

NUCLEO-H743ZI replaced with NUCLEO-H743ZI2, you can refer to the STM32 Nucleo (144 pins) schematics 1.1.

Have a look at this UM1974 User manual STM32 Nucleo-144 boards (MB1137) for Ordering information.

Edit : the schematic file MB1364-H743ZI-C01 Schematics 1.0

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Nikita91
Lead II

Strange...

Schematics 1.1 is MB1137 rev B-01 from 2015, with STLINK V2-1

Schematics MB1364-H743ZI-C01 Schematics 1.0 is MB1364 rev C-01 from 2018, with STLINK V3

Thanks, this seems to be the schematic for NUCLEO-H743ZI2

Oups, sorry ! I'm pointed on the wrong file.

Thanks @Nikita91​  for providing the right schematic file.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen