2020-11-17 01:33 AM
Only schematic of STM32H743ZI is available, not for STM2H743ZI2, how can I get schematic diagram of STM2H743ZI2 ?
Solved! Go to Solution.
2020-11-17 03:34 AM
Strange...
Schematics 1.1 is MB1137 rev B-01 from 2015, with STLINK V2-1
Schematics MB1364-H743ZI-C01 Schematics 1.0 is MB1364 rev C-01 from 2018, with STLINK V3
2020-11-17 03:18 AM
Hello @PREDATOR ,
NUCLEO-H743ZI replaced with NUCLEO-H743ZI2, you can refer to the STM32 Nucleo (144 pins) schematics 1.1.
Have a look at this UM1974 User manual STM32 Nucleo-144 boards (MB1137) for Ordering information.
Edit : the schematic file MB1364-H743ZI-C01 Schematics 1.0
Imen
2020-11-17 03:34 AM
Strange...
Schematics 1.1 is MB1137 rev B-01 from 2015, with STLINK V2-1
Schematics MB1364-H743ZI-C01 Schematics 1.0 is MB1364 rev C-01 from 2018, with STLINK V3
2020-11-17 04:01 AM
Thanks, this seems to be the schematic for NUCLEO-H743ZI2
2020-11-17 04:36 AM
Oups, sorry ! I'm pointed on the wrong file.
Thanks @Nikita91 for providing the right schematic file.
Imen