2024-06-28 2:16 AM
Please confirm the default state of BOOT1 pin state through nBOOT1 bit for BOOT configuration. How can we pre-configure nBOOT1 bit for BOOT configuration?
2024-06-28 7:33 AM
You can read and set the configuration by STM32CubeProgrammer.
hth
KnarfB
2024-06-28 7:47 AM
Hello sbhowmick94,
The default state of the nBOOT1 bit for BOOT configuration is set to 1, it's written in the RM0351 :
and like KnarfB said you can set the configurations in STM32CubeProgrammer.
Regards,
Stassen
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.