2020-09-02 04:39 AM
I am experiencing a bug in the ST-Link FW V2.J37.M26
setup
Nucleo-F446RE power from E5V
it takes a long time to "boot" or start to execute code. some code will never start running. the problem goes away if the ST-Link is power from USB before E5V is turn on
I have captured the problem on the scope. The MCO clock from ST-Link stops for about 2sek when power from E5V.
Nucleo-F446RE power from E5V ST-Link FW V2.J37.M26
Blu E5V
Yellow T_NRST
Pink MCO
Nucleo-F446RE power from USB ST-Link FW V2.J37.M26
Blu E5V
Yellow T_NRST
Pink MCO
Nucleo-F446RE power from E5V ST-Link FW V2.J34.M25
Blu E5V
Yellow T_NRST
Pink MCO
Note the the time division is different
The following FW versions are bug free
V2.J33.M25
V2.J34.M25
V2.J35.M26
I am curious
Why have ST chosen to gennerat the clock from the ST-Link MCU?
Best regards
Martin
2020-09-02 05:54 AM
>>I am curious. Why have ST chosen to generate the clock from the ST-Link MCU?
To save a crystal in the design.
You can add one if you want, or equally chose to use the HSI source rather than the HSE
2021-05-19 01:07 AM
I have a Nucleo-F207ZG board and I am facing the same problem: if you power the board from E5V or VIN, MCO starts to oscillate after approx 2 seconds when NRST signal is already high. Because of this wrong start-up sequence, most of codes will never start to run. The only solution is to manually reset the board after 2 seconds from power-up.
This problem doesn't happen if you power the board from the USB connector of the ST-LINK.
In addition to the original post, also the following FW versions have this bug:
V2.37.27
V2.38.27
Please, let us know if you implement a solution in the future ST-LINK firmware releases.
Thanks.
Regards,
Riccardo
2022-09-23 10:07 AM
Good day, do you know of any link to download the st-link with firmware V2.J34.M25 or V2.J35.M26? Greetings.
2022-09-23 10:20 AM