cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with V_BAT Connection on Custom STM32F407VGT6 Board

rohithinthingstech
Associate II

Hello everyone,

I have designed a custom board using the STM32F407VGT6, and I have connected a 3V coin cell battery (CR2032) to the V_BAT pin as shown in the schematic below:

V_BAT Circuit Details:

  • A 3V battery is directly connected to the V_BAT pin.
  • A 0.1µF capacitor (C14) is placed across V_BAT and GND.
  • V_BAT is connected directly to the STM32.

However, I am facing an issue where I do not measure any voltage at the V_BAT pin on my board. It seems like the battery is not supplying power to the backup domain.

  1. Why am I not getting voltage on the V_BAT pin?
  2. Are there any hardware design issues with my schematic?
  3. Is there any special configuration required in firmware to enable the backup domain power?

I have attached my schematic for reference.

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

> do not measure any voltage at the V_BAT pin on my board

A multimeter across the battery should show voltage. If using the ADC, show relevant code. Should be getting something. Nothing wrong with the schematic snippet.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
mÆŽALLEm
ST Employee

Hello,

You can refer to the STM32F4G EVAL schematics:

As you can see nothing special:

mALLEm_1-1741008002938.png

For the code you can refer to the RTC calendar example here.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
TDK
Guru

> do not measure any voltage at the V_BAT pin on my board

A multimeter across the battery should show voltage. If using the ADC, show relevant code. Should be getting something. Nothing wrong with the schematic snippet.

If you feel a post has answered your question, please click "Accept as Solution".

 

You can paste the image directly into the post - where we can see it:

AndrewNeil_0-1741012784009.png


@rohithinthingstech wrote:

I do not measure any voltage at the V_BAT pin on my board. It seems like the battery is not supplying power to the backup domain.


Is the battery dead?

Have you measured to see if current is being drawn from the battery?

 

@rohithinthingstech wrote:

I have designed a custom board .


Have you checked the layout for shorts?

Have you checked the assembly for shorts and bad joints?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.