cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to use STLink-V3 mini for serial interface?

SRAHM.1
Associate

Using the EVALKIT-Robot-1 which is based on STSPIN32F0A. I am using the STLink-V3-mini rather than the RS485. I want to know if it is possible to establish serial communication through UART with the STLink V3.

1 REPLY 1
Pavel A.
Evangelist III

The serial (VCP) part of the st-link works independently of the debugger part.

You can connect TTL UART pins to it.