2022-12-14 1:24 AM
I read on the intenet that they both are used to debug the IC.
But how they differ?
thanks
Solved! Go to Solution.
2023-01-24 2:49 AM
Hello @YShko.1,
ST-Link is a hardware debug probe
JTAG is a standard protocol.
ST-Link is used to debug STM32 microcontrollers while JTAG is a standard protocol used to debug a wide range of microcontrollers.
You can also refer to this AN4989 to learn more about it!
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-14 1:37 AM
ST-Link is a hardware debug probe, as J-Link and I-Jet.
Most debug probe support 2 type of debug bus, the standard JTAG and the Arm 2+ wire SWD interface. Some debug probe support additonal debug feature such as virtual port com, trace, etc....
2023-01-24 2:24 AM
Hey,
So base on your answare ST-LINK is a hardware debug probe which has a JTAG bus?
2023-01-24 2:49 AM
Hello @YShko.1,
ST-Link is a hardware debug probe
JTAG is a standard protocol.
ST-Link is used to debug STM32 microcontrollers while JTAG is a standard protocol used to debug a wide range of microcontrollers.
You can also refer to this AN4989 to learn more about it!
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.