cancel
Showing results for 
Search instead for 
Did you mean: 

In the schematic of STM32F030F4, the capacitor values are written 104, what is the unit of it?

Prajnyajit
Associate II

I chose STM32F030F4 as MCU for my device. I have gone through its schematic (attached for reference). I have little doubt about it. The capacitor values are written 104, that's it. Please help me find its unit, I will be too much helpful.

Secondly, I have to connect two components to its PA9 (SCL/TX), and PA10 (SDA/RX). How to code them, because both will be connected to the same pins so will it cause an error?

0693W00000LydRPQAZ.png

11 REPLIES 11

As KnarfB said - AN4325 is the primary reference. And then, of course, all of the ST's Nucleo, Discovery and Evaluation boards also.