cancel
Showing results for 
Search instead for 
Did you mean: 

ILI9488 -TFT (without touch) not working on STM32H563ZIT6

Berlin-raj123
Associate II

Hi, I am trying to interface with a 3.5-inch ILI9488 TFT display (without touch) on an STM32H563ZIT6 microcontroller. I'm attempting to write a test function to fill the entire screen with a solid red color, but it's not working. Could anyone please help me? I will attach my code. How can I verify that SPI is properly working with the TFT?

#include "main.h"

SPI_HandleTypeDef hspi2;

UART_HandleTypeDef huart7;

#define ILI9488_CMD_MEMORY_WRITE        0x2C
#define ILI9488_CMD_MEMORY_ACCESS_CTRL  0x36

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_ICACHE_Init(void);
static void MX_SPI2_Init(void);
static void MX_UART7_Init(void);
void ILI9488_FillScreen(uint16_t color);
void ILI9488_SendData(uint8_t data);
void ILI9488_SendCommand(uint8_t cmd);
void ILI9488_Init(void);
void testFillScreen(uint16_t color);

#define WIDTH  320
#define HEIGHT 480
#define CS_PORT GPIOB
#define CS_PIN    GPIO_PIN_12

#define DC_PORT GPIOE
#define DC_PIN    GPIO_PIN_4

#define RESET_PORT GPIOE
#define RESET_PIN GPIO_PIN_2
uint8_t tx_buffer[50];
int uart_buffer_len;
char spi_buffer[20];
int main(void)
{
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
/* Configure the system clock */
  SystemClock_Config();
/* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_ICACHE_Init();
  MX_SPI2_Init();
  MX_UART7_Init();
  ILI9488_Init();
  // Test filling screen with red color
  ILI9488_FillScreen(0xF800); // Red color in 16-bit RGB
  while (1)
  {

  }
}
void ILI9488_Init(void)
{
	 // Reset display
    ILI9488_SendCommand(0x01); // Software Reset
    HAL_Delay(150);
    ILI9488_SendCommand(0x11); // Sleep Out
    HAL_Delay(150);
    ILI9488_SendCommand(0x29); // Display On
}
void ILI9488_SendCommand(uint8_t cmd)
{
    HAL_GPIO_WritePin(GPIOE, GPIO_PIN_4, GPIO_PIN_RESET); // DC low for command
    HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_RESET); // CS low
    HAL_SPI_Transmit(&hspi2, &cmd, 1, HAL_MAX_DELAY);
    HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_SET);   // CS high
}
void ILI9488_FillScreen(uint16_t color)
{
    uint8_t highByte = color >> 8;
    uint8_t lowByte = color & 0xFF;

    ILI9488_SendCommand(0x2C); // Memory Write

    for (int i = 0; i < WIDTH * HEIGHT; i++)
    {
        ILI9488_SendData(highByte);
        ILI9488_SendData(lowByte);
    }
}
void ILI9488_SendData(uint8_t data)
{
    HAL_GPIO_WritePin(GPIOE, GPIO_PIN_4, GPIO_PIN_SET);   // DC high for data
    HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_RESET); // CS low
    HAL_SPI_Transmit(&hspi2, &data, 1, HAL_MAX_DELAY);
    HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_SET);   // CS high
}
22 REPLIES 22
MasterT
Lead

Try to locate arduino library for ILI9488, study init procedure.

To verify connection read back internal registers, ID, etc, and verify.

@MasterT Can you refer any Arduino library related to a 3.5-inch ILI9488 TFT without touch?

I showed you here:

https://community.st.com/t5/stm32-mcus-boards-and-hardware/ili9488-tft-example-code-in-stm32h563zit6/td-p/688509

But no answer...nothing.

Which you choose ? or why not using this examples ?

If you feel a post has answered your question, please click "Accept as Solution".

@AScha.3 

https://community.st.com/t5/stm32-mcus-boards-and-hardware/ili9488-tft-example-code-in-stm32h563zit6/td-p/688509

In this example, the configuration is done using STM32CubeMX, and the settings and configuration are different. I am unable to understand it, but I am using STM32CubeIDE. 

>but I am using STM32CubeIDE

me too. 

>the configuration is done using STM32CubeMX

yes, its exactly same.

>am unable to understand it

ok, so this might be more easy to understand:

https://github.com/timagr615/TFT_ILI9488

(it is from the search/list i posted, so why you dont use it / try it ?? )

If you feel a post has answered your question, please click "Accept as Solution".

thank you @AScha.3 for your support, i will try

HI, @AScha.3  I tried the ILI9488 TFT, but it's not working. I have a doubt about the SPI configuration. I will send my IOC configuration as well as the code for sending a single command to the TFT through SPI. and I am checking the MOSI pin using an oscilloscope, but it is not showing any signal. I want to be aware of the SPI configuration.

help me!

#define RESET_PIN GPIO_PIN_2
#define RESET_PORT GPIOE
#define DC_PIN GPIO_PIN_4
#define DC_PORT GPIOE
#define CS_PIN GPIO_PIN_12
#define CS_PORT GPIOB
int main(void)
{
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
  SystemClock_Config();
  MX_GPIO_Init();
  MX_ICACHE_Init();
  MX_UART7_Init();
  MX_SPI2_Init();
  //MIPI-DBI Type C Option 3 (4-line SPI)
  HAL_GPIO_WritePin(GPIOF,GPIO_PIN_8,SET);//IM0--->1
  HAL_GPIO_WritePin(GPIOF,GPIO_PIN_9,SET);IM1--->1
  HAL_GPIO_WritePin(GPIOF,GPIO_PIN_10,SET);IM2--->1
  TFT_init();
  while (1)
  {
	  ILI9488_SendCommand(0xE);      // Adjust Control
	  HAL_Delay(1000);
  }
}
void TFT_init()
{
	HAL_GPIO_WritePin(CS_PORT,CS_PIN,GPIO_PIN_SET);
	HAL_GPIO_WritePin(RESET_PORT,RESET_PIN,GPIO_PIN_SET);
	HAL_Delay(1); // Delay 1ms
	HAL_GPIO_WritePin(RESET_PORT,RESET_PIN,GPIO_PIN_RESET);
	HAL_Delay(10); // Delay 10ms // This delay time is necessary
	HAL_GPIO_WritePin(RESET_PORT,RESET_PIN,GPIO_PIN_SET);
	HAL_Delay(120); // Delay 100 ms
}
void ILI9488_SendCommand(uint8_t com)
{
	//*(__IO uint8_t *)(0x60000000) = com;
	uint8_t tmpCmd = com;
	//Set DC HIGH for COMMAND mode
	//HAL_GPIO_WritePin(tftDC_GPIO, tftDC_PIN, GPIO_PIN_RESET);
	HAL_GPIO_WritePin(DC_PORT,DC_PIN,GPIO_PIN_RESET);
	//Put CS LOW
	//HAL_GPIO_WritePin(tftCS_GPIO, tftCS_PIN, GPIO_PIN_RESET);
	HAL_GPIO_WritePin(CS_PORT,CS_PIN,GPIO_PIN_RESET);
	//Write byte using SPI
	HAL_SPI_Transmit(&hspi2, &tmpCmd, 1, 1);
	//SendByte(tmpCmd);
	//WaitLastData();
	HAL_GPIO_WritePin(CS_PORT,CS_PIN,GPIO_PIN_SET);
	//Bring CS HIGH
	//HAL_GPIO_WritePin(tftCS_GPIO, tftCS_PIN, GPIO_PIN_SET);
}
static void MX_SPI2_Init(void)
{
  /* USER CODE END SPI2_Init 1 */
  /* SPI2 parameter configuration*/
  hspi2.Instance = SPI2;
  hspi2.Init.Mode = SPI_MODE_MASTER;
  hspi2.Init.Direction = SPI_DIRECTION_2LINES;
  hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
  hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
  hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
  hspi2.Init.NSS = SPI_NSS_SOFT;
  hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_128;
  hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
  hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
  hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
  hspi2.Init.CRCPolynomial = 0x7;
  hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
  hspi2.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
  hspi2.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
  hspi2.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
  hspi2.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
  hspi2.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
  hspi2.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
  hspi2.Init.IOSwap = SPI_IO_SWAP_DISABLE;
  hspi2.Init.ReadyMasterManagement = SPI_RDY_MASTER_MANAGEMENT_INTERNALLY;
  hspi2.Init.ReadyPolarity = SPI_RDY_POLARITY_HIGH;
  if (HAL_SPI_Init(&hspi2) != HAL_OK)
  {
    Error_Handler();
  }
}

Screenshot 2024-07-18 191011.pngScreenshot 2024-07-18 190939.pngScreenshot 2024-07-18 191227.png

 

 

1. Is this

AScha3_0-1721310694818.png

according to the ds of ILI9488 ?

If you feel a post has answered your question, please click "Accept as Solution".

Screenshot 2024-07-19 180100.png