cancel
Showing results for 
Search instead for 
Did you mean: 

I made a prototype board using STM32H7A3LIH6Q. Before the firmware was written, a current of 500mA flowed(@+3.3V).

DE.1
Associate II

I made a prototype board using STM32H7A3LIH6Q.

Before the firmware was written, a current of 500mA flowed(@+3.3V).

VDD and VSS were not shorted.

Q1)Have there been such cases in the past?

Q2)Are there any mistakes in the wiring of the circuit?

Q3)VFBSMPS is plane on the inner layer of the board, is there any problem?

1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Chief III

is C48 correct there ? 100nF ? :*

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

8 REPLIES 8

Does seem excessive, is that the point the supply limits out?

Not sure what the expectations are when it thinks its in LDO mode, or what the ROM software does.

Perhaps find a local FAE you can discuss with.

In the mean time walk the schematic and check the pin/ball assignments again.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

VDD_LDO shouldn't connect to 3V3, its the same node a VCAP / VFBSMPS

Perhaps look at H7B3I-DK schematic

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
DE.1
Associate II

Thank you for your reply.

I looked at the H7B3I-DK schematic.

I understand there is a difference with the H7B3I-DK schematic.

When I set SMPS and LDO to [SMPS_2V5_SUPPLY_LDO], I observed 3.3V, 0.05A.

When I set SMPS and LDO to [POWER_LDO_SUPPLY], I observed 3.3V, 0.05A.

There was a 10x difference.

I'm thinking the problem is because when I have the LDO set it consumes less power than when I have the SMPS set.

I think I'm doing something serious wrong, but I don't know why.

DE.1
Associate II

Sorry, ​I made a mistake.

Below are the measurement results.

When I set SMPS and LDO to [SMPS_2V5_SUPPLY_LDO], I observed 3.3V, 0.5A.

When I set SMPS and LDO to [POWER_LDO_SUPPLY], I observed 3.3V, 0.05A.

AScha.3
Chief III

is C48 correct there ? 100nF ? :*

If you feel a post has answered your question, please click "Accept as Solution".

Thank you for your reply.

The value was wrong.

After fixing the capacitor, the current value decreased.

Thank you for your pointing out.

LCE
Principal II

Wow, 100 nF at the switching output!

Amazing, and a good sign for the SMPS's robustness that it survived that!

Tesla pointed out another flaw...

And just in case you don't know, there is AN5307.