2022-12-15 8:30 AM
I have STM32H7A3ZITXQ_RAM.ld in NUCLEO-STM32H7A3 Board.
I need to know what is the procedure to download and run project from Internal SRAM completely of STM32H7A3 Nucleo(144)Board.
I built Base Default Nucleo-H7A3 STM32 Board .ioc Project in STM32Cube IDE.
When I debug using onboard ST-Link Debugger, It start running from SRAM,
But after few stepping or F6, trying to run somewhere I am getting unable to open disassembly file.
2022-12-15 9:16 AM
Has it built correctly for the address of the RAM? Check the .MAP file.
Have you modified SystemInit() to configure the SCB->VTOR with the correct vector table address? I'd use a linker symbol myself, but ST uses a #define for reasons that defy logic.
>>But after few stepping or F6, trying to run somewhere I am getting unable to open disassembly file.
So it does enter your code, and ResetHandler? main()? at what point does it disappear into a black hole?
If you stop the debugger, where is it executing?